NXP Reader Library  v17.1.0.2535
Application Layer

Contains Application specific implementations for various contactless cards like ULTRALIGHT, CLASSIC, Plus, DESFire and so on... More...

Collaboration diagram for Application Layer:

Modules

 MIFARE(R) Classic
 These Functions implement the MIFARE(R) Classic commands.
 
 MIFARE DESFire (R)
 These Functions implement the MIFARE DESFire(R) EV1 commands.
 
 MIFARE DESFire EVx
 These Functions implement the MIFARE DESFire EVx commands.
 
 MIFARE DESFire Light
 These Functions implement the MIFARE DESFire Light commands.
 
 MIFARE DUOX
 This is only a wrapper layer to abstract the different MIFARE DUOX implementations. With this wrapper it is possible to support more than one MIFARE DUOX implementation in parallel, by adapting this wrapper.
 
 Felica
 These Components implement the Felica commands.
 
 ICode
 Generic component that provides the command description of ICode products.
 
 ISO/IEC 18000-3 Mode3
 These Components implement the ICODE ILT support.
 
 NTAG 42x DNA / TT
 These Functions implement the NTAG 42x DNA / TT commands.
 
 NTAG X DNA
 This is only a wrapper layer to abstract the different NTAG X DNA implementations. With this wrapper it is possible to support more than one NTAG X DNA implementation in parallel, by adapting this wrapper.
 
 MIFARE Plus (R)
 These Components implement the MIFARE Plus (R) commands.
 
 MIFARE Plus EVx
 These Components implement the MIFARE Plus (EVx, EV2, future versions) commands.
 
 MIFARE PRIME NTAG
 These Functions implement the MIFARE PRIME NTAG commands.
 
 MIFARE(R) Ultralight
 This is only a wrapper layer to abstract the different MIFARE Ultralight / NTAG implementations. With this wrapper it is possible to support more than one MIFARE Ultralight / NTAG implementation in parallel, by adapting this wrapper.
 
 Virtual Card Architecture (R)
 These Components implement the Virtual Card Architecture (R) commands.
 

Detailed Description

Contains Application specific implementations for various contactless cards like ULTRALIGHT, CLASSIC, Plus, DESFire and so on...