NXP Reader Library  v17.1.0.2535

Describes about the macro definitions supported / to be used in the interfaces. More...

Collaboration diagram for Defines:

Modules

 Buffer Size
 
 Flags
 Description about the Request Flags.
 
 Options
 Description for Option definitions that will be used in Mandatory, Optional and Custom set of commands. When these definitions are used it will update the Flags 7th bit (PHAL_ICODE_FLAG_OPTION)
 

Detailed Description

Describes about the macro definitions supported / to be used in the interfaces.