NXP Reader Library  v17.1.0.2535

Description of options to be used for Custom command sets. More...

Collaboration diagram for Defines:

Modules

 ExtendedInventoryFlags
 Options to be used with InventoryReadExtended command.
 
 Password
 Password option for the below interfaces.
 
 ProtectPage
 Describes the definitions for ProtectPage command.
 
 BitRates
 BitRate Options to be used for below interfaces.
 
 Timing
 Timing Options to be used for below interfaces.
 

Detailed Description

Description of options to be used for Custom command sets.