NXP Reader Library  v17.1.0.2535

Description about the Request Flags. More...

Collaboration diagram for Flags:

Modules

 Common
 Flags that are common and are part of bits 1 - 4 ( i.e. 0 - 3). These flags will be utilized for the below mentioned interfaces.
 
 Inventory_NotSet
 Flags when Inventory is NOT SET. These are part for bits 5 - 8 ( i.e. 4 - 7). These flags will be utilized for the below mentioned interfaces.
 
 Inventory_Set
 Flags when Inventory is SET. These are part for bits 5 - 8 ( i.e. 4 - 7). These flags will be utilized for the below mentioned interfaces.
 

Detailed Description

Description about the Request Flags.