Flags that are common and are part of bits 1 - 4 ( i.e. 0 - 3). These flags will be utilized for the below mentioned interfaces. More...

Macros | |
| #define | PHAL_ICODE_FLAG_TWO_SUB_CARRIERS 0x01U |
| Sub-Carrier Flag. More... | |
| #define | PHAL_ICODE_FLAG_DATA_RATE 0x02U |
| DataRate Flag. More... | |
| #define | PHAL_ICODE_FLAG_INVENTORY 0x04U |
| Inventory Flag. More... | |
| #define | PHAL_ICODE_FLAG_PROTOCOL_EXTENSION 0x08U |
| ProtocolExtension Flag. More... | |
| #define | PHAL_ICODE_FLAG_OPTION 0x40U |
| Option Flag. More... | |
| #define | PHAL_ICODE_FLAG_FAST_DATA_RATE 0x80U |
| RFU as per ISO15693 but this flag should be utilized for NTAG5 product only. More... | |
Flags that are common and are part of bits 1 - 4 ( i.e. 0 - 3). These flags will be utilized for the below mentioned interfaces.
| #define PHAL_ICODE_FLAG_TWO_SUB_CARRIERS 0x01U |
Sub-Carrier Flag.
If set two sub-carriers shall be used (VICC to VCD). Else a single sub-carrier frequency shall be used by the VICC.
| #define PHAL_ICODE_FLAG_DATA_RATE 0x02U |
DataRate Flag.
If set high data rate shall be used (VICC to VCD). Else low data rate shall be used.
| #define PHAL_ICODE_FLAG_INVENTORY 0x04U |
Inventory Flag.
Shall be set for inventory request. Refer below sub flags in case of Inventory is set or not set.
| #define PHAL_ICODE_FLAG_PROTOCOL_EXTENSION 0x08U |
ProtocolExtension Flag.
If set protocol format is extended. Reserved for future use. No supported in current version.
| #define PHAL_ICODE_FLAG_OPTION 0x40U |
Option Flag.
Meaning is defined by the command description. It shall be set to 0 if not otherwise defined by the command.
| #define PHAL_ICODE_FLAG_FAST_DATA_RATE 0x80U |
RFU as per ISO15693 but this flag should be utilized for NTAG5 product only.
This flag is used to set the hardware RX DataRate to Fast_High (~53 kbps) for Fast_Low (~13 kbps). Also to note that this flag should not be used for any Inventory commands. Currently the support is for