NXP Reader Library  v17.1.0.2535
Inventory_Set

Flags when Inventory is SET. These are part for bits 5 - 8 ( i.e. 4 - 7). These flags will be utilized for the below mentioned interfaces. More...

Collaboration diagram for Inventory_Set:

Macros

#define PHAL_ICODE_FLAG_AFI   0x10U
 AFI Flag. More...
 
#define PHAL_ICODE_FLAG_NBSLOTS   0x20U
 NbSlots Flag. More...
 

Detailed Description

Flags when Inventory is SET. These are part for bits 5 - 8 ( i.e. 4 - 7). These flags will be utilized for the below mentioned interfaces.

Macro Definition Documentation

◆ PHAL_ICODE_FLAG_AFI

#define PHAL_ICODE_FLAG_AFI   0x10U

AFI Flag.

If set AFI field is present in request. If not set AFI field is not present in request.

◆ PHAL_ICODE_FLAG_NBSLOTS

#define PHAL_ICODE_FLAG_NBSLOTS   0x20U

NbSlots Flag.

If set Use 1 slot instead of 16 slots for inventory. If not set use 16 slots.