The Options to indicate the file targeted is a CRLFile or not. To be used for below mentioned interface. ReadData WriteData. More...

Macros | |
| #define | PHAL_MFDUOX_TARGET_FILE_CRLFILE 0x01 |
| Option to represent the native chaining format. More... | |
The Options to indicate the file targeted is a CRLFile or not. To be used for below mentioned interface. ReadData WriteData.
| #define PHAL_MFDUOX_TARGET_FILE_CRLFILE 0x01 |
Option to represent the native chaining format.
Here AF will be available as command code in Command and Response.