NXP Reader Library  v17.1.0.2535

Error Codes received from PICC and the equivalent Reader Library error codes. More...

Collaboration diagram for ErrorCodes:

Modules

 ErrorCodes_PICC
 The actual error codes received from PICC. These codes are for reference purpose only. All the interfaces will return codes mentioned in Mapped Codes and not these codes.
 
 ErrorCodes_Mapped
 The error codes from Library with respect to PICC Error codes.
 

Detailed Description

Error Codes received from PICC and the equivalent Reader Library error codes.