NXP Reader Library  v17.1.0.2535

The actual error codes received from PICC. These codes are for reference purpose only. All the interfaces will return codes mentioned in Mapped Codes and not these codes. More...

Collaboration diagram for ErrorCodes_PICC:

Modules

 Native
 MIFARE DUOX Native Response Codes.
 
 ISO7816
 MIFARE DUOX Native ISO 7816 Response Codes.
 

Detailed Description

The actual error codes received from PICC. These codes are for reference purpose only. All the interfaces will return codes mentioned in Mapped Codes and not these codes.