Macro Definitions for File Management commands. More...

Modules | |
| FileOptions | |
| The File Options to be used for all the File management commands. | |
| LimitedCredit | |
| The File Options to be used for Create Value File interface. | |
| GetValue | |
| The File Options to be used for Create Value File interface. | |
| DiversificationOption | |
| The Diversification Options to be used for Create Transaction MAC File interface. | |
| TMKeyOptions | |
| The TMKey Options to be used for Create Transaction MAC File interface. | |
| CommandCodes | |
Macro Definitions for File Management commands.