These Components implement the MIFARE NTAG 42xDNA File Management related commands.
More...
|
| phStatus_t | phalMfNtag42XDna_GetFileSettings (void *pDataParams, uint8_t bFileNo, uint8_t *pFSBuffer, uint8_t *bBufferLen) |
| | Get informtion on the properties of a specific file. More...
|
| |
| phStatus_t | phalMfNtag42XDna_GetFileCounters (void *pDataParams, uint8_t bOption, uint8_t bFileNo, uint8_t *pFileCounters, uint8_t *pRxLen) |
| | Returns manufacturing related data of the PICC. More...
|
| |
| phStatus_t | phalMfNtag42XDna_ChangeFileSettings (void *pDataParams, uint8_t bCommMode, uint8_t bFileNo, uint8_t bFileOption, uint8_t *pAccessRights, uint8_t bAdditionalInfoLen, uint8_t *bAdditionalInfo) |
| | Changes the access parameters of an existing file. More...
|
| |
| phStatus_t | phalMfNtag42XDna_ChangeFileSettingsSDM (void *pDataParams, uint8_t bOption, uint8_t bFileNo, uint8_t bFileOption, uint8_t *pAccessRights, uint8_t bSdmOptions, uint8_t *pSdmAccessRights, uint8_t *pVCUIDOffset, uint8_t *pSDMReadCtrOffset, uint8_t *pPICCDataOffset, uint8_t *pTTPermStatusOffset, uint8_t *pSDMMACInputOffset, uint8_t *pSDMENCOffset, uint8_t *pSDMENCLen, uint8_t *pSDMMACOffset, uint8_t *pSDMReadCtrLimit) |
| | Changes the access parameters of an existing file. More...
|
| |
These Components implement the MIFARE NTAG 42xDNA File Management related commands.
◆ phalMfNtag42XDna_GetFileSettings()
Get informtion on the properties of a specific file.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bFileNo | [In] The file number for which the setting to be retrieved. |
| [out] | pFSBuffer | [Out] The buffer containing the settings. The buffer should be 17 bytes. |
| [out] | bBufferLen | [Out] The length of bytes available in FSBuffer buffer. |
◆ phalMfNtag42XDna_GetFileCounters()
Returns manufacturing related data of the PICC.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bOption | [In] Indicates the mode of communication to be used while exchanging the data to PICC.
|
| [in] | bFileNo | [In] File number for which the Counter information need to be received. |
| [out] | pFileCounters | [Out] The SDMReadCounter information returned by the PICC. |
| [out] | pRxLen | [Out] Length of bytes available in FileCounters buffer. |
◆ phalMfNtag42XDna_ChangeFileSettings()
Changes the access parameters of an existing file.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bCommMode | [In] Indicates the mode of communication to be used while exchanging the data to PICC.
|
| [in] | bFileNo | [In] File number for which the setting need to be updated. |
| [in] | bFileOption | [In] New communication settings for the file.
|
| [in] | pAccessRights | [In] The new access right to be applied for the file. Should be 2 byte. |
| [in] | bAdditionalInfoLen | [In] Length of the Additional Info to be sent (2 Bytes or 4 Bytes). This is used to set TMC Limit in case of TMAC File |
| [in] | bAdditionalInfo | [In] One of the below inforamtion.
If Standard AES: 4 byte TMC Limit value.
If LRP : 2 byte TMC Limit value. |
◆ phalMfNtag42XDna_ChangeFileSettingsSDM()
| phStatus_t phalMfNtag42XDna_ChangeFileSettingsSDM |
( |
void * |
pDataParams, |
|
|
uint8_t |
bOption, |
|
|
uint8_t |
bFileNo, |
|
|
uint8_t |
bFileOption, |
|
|
uint8_t * |
pAccessRights, |
|
|
uint8_t |
bSdmOptions, |
|
|
uint8_t * |
pSdmAccessRights, |
|
|
uint8_t * |
pVCUIDOffset, |
|
|
uint8_t * |
pSDMReadCtrOffset, |
|
|
uint8_t * |
pPICCDataOffset, |
|
|
uint8_t * |
pTTPermStatusOffset, |
|
|
uint8_t * |
pSDMMACInputOffset, |
|
|
uint8_t * |
pSDMENCOffset, |
|
|
uint8_t * |
pSDMENCLen, |
|
|
uint8_t * |
pSDMMACOffset, |
|
|
uint8_t * |
pSDMReadCtrLimit |
|
) |
| |
Changes the access parameters of an existing file.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bOption | [In] Indicates the mode of communication to be used while exchanging the data to PICC.
|
| [in] | bFileNo | [In] File number for which the setting need to be updated. |
| [in] | bFileOption | [In] New communication settings for the file.
|
| [in] | pAccessRights | [In] The new access right to be applied for the file. Should be 2 byte. |
| [in] | bSdmOptions | [In] One of the below values to be used. Can be ORed.
|
| [in] | pSdmAccessRights | [In] The SDM access rights to be applied. Should be 2 bytes. |
| [in] | pVCUIDOffset | [In] VCUID Offset information. Should be 3 bytes. |
| [in] | pSDMReadCtrOffset | [In] SDMReadCtr value (LSB first). Should be 3 bytes. |
| [in] | pPICCDataOffset | [In] Mirror position (LSB first) for encrypted PICCData. Should be 3 bytes. |
| [in] | pTTPermStatusOffset | [In] Tag Tamper Permanent Status Offset value. Should be 3 bytes. |
| [in] | pSDMMACInputOffset | [In] Offset in the file where the SDM MAC computation starts (LSB first). Should be 3 bytes. |
| [in] | pSDMENCOffset | [In] SDMENCFileData mirror position (LSB first). Should be 3 bytes. |
| [in] | pSDMENCLen | [In] Length of the SDMENCFileData (LSB first). Should be 3 bytes. |
| [in] | pSDMMACOffset | [In] SDMMAC mirror position (LSB first). Should be 3 bytes. |
| [in] | pSDMReadCtrLimit | [In] SDM Read Counter Limit value. Should be 3 bytes. |