These Components implement the MIFARE NTAG 42xDNA ISO/IEC 7816-4 Basic commands.
More...
|
| phStatus_t | phalMfNtag42XDna_IsoSelectFile (void *pDataParams, uint8_t bOption, uint8_t bSelector, uint8_t *pFid, uint8_t *pDFname, uint8_t bDFnameLen, uint8_t bExtendedLenApdu, uint8_t **ppFCI, uint16_t *pwFCILen) |
| | ISO Select. More...
|
| |
| phStatus_t | phalMfNtag42XDna_IsoReadBinary (void *pDataParams, uint16_t wOption, uint8_t bOffset, uint8_t bSfid, uint32_t dwBytesToRead, uint8_t bExtendedLenApdu, uint8_t **ppRxBuffer, uint32_t *pBytesRead) |
| | ISO Read Binary. More...
|
| |
| phStatus_t | phalMfNtag42XDna_IsoUpdateBinary (void *pDataParams, uint8_t bOffset, uint8_t bSfid, uint8_t bExtendedLenApdu, uint8_t *pData, uint32_t dwDataLen) |
| | Iso Update Binary. More...
|
| |
These Components implement the MIFARE NTAG 42xDNA ISO/IEC 7816-4 Basic commands.
◆ PHAL_MFNTAG42XDNA_SELECTOR_2
| #define PHAL_MFNTAG42XDNA_SELECTOR_2 0x02U |
Option to indicate Select EF under current DF.
Fid = EF id.
◆ PHAL_MFNTAG42XDNA_SELECTOR_4
| #define PHAL_MFNTAG42XDNA_SELECTOR_4 0x04U |
Option to indicate Selection by DF Name.
DFName and len is then valid.
◆ phalMfNtag42XDna_IsoSelectFile()
ISO Select.
This command is implemented in compliance with ISO/IEC 7816-4.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bOption | [In] Option for return / no return of FCI.
|
| [in] | bSelector | [In] The selector to be used.
|
| [in] | pFid | [In] The ISO File number to be selected. |
| [in] | pDFname | [In] The ISO DFName to be selected. Valid only when bOption = 0x04. |
| [in] | bDFnameLen | [In] Length of bytes available in DFname buffer. |
| [in] | bExtendedLenApdu | [In] Flag for Extended Length APDU. This should be always cleared |
| [out] | ppFCI | [Out] The FCI information returned by the PICC. |
| [out] | pwFCILen | [Out] Length of bytes available in FCI buffer. |
◆ phalMfNtag42XDna_IsoReadBinary()
ISO Read Binary.
This command is implemented in compliance with ISO/IEC 7816-4.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | wOption | [In] One of the below options.
|
| [in] | bOffset | [In] The offset from where the data should be read. |
| [in] | bSfid | [In] Short ISO File Id. Bit 7 should be 1 to indicate Sfid is supplied. Else it is treated as MSB of 2Byte offset. |
| [in] | dwBytesToRead | [In] Number of bytes to read. If 0, then entire file to be read. |
| [in] | bExtendedLenApdu | [In] Flag for Extended Length APDU. This should be always cleared |
| [out] | ppRxBuffer | [Out] The data retuned by the PICC. |
| [out] | pBytesRead | [Out] Length of bytes available in RxData buffer. |
◆ phalMfNtag42XDna_IsoUpdateBinary()
Iso Update Binary.
This command is implemented in compliance with ISO/IEC 7816-4.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bOffset | [In] The offset from where the data should be updated. |
| [in] | bSfid | [In] Short ISO File Id. Bit 7 should be 1 to indicate Sfid is supplied. Else it is treated as MSB of 2Byte offset. |
| [in] | bExtendedLenApdu | [In] Flag for Extended Length APDU. This should be always cleared |
| [in] | pData | [In] Data to be updated. |
| [in] | dwDataLen | [In] Length of bytes available in Data buffer. |