NXP Reader Library  v17.1.0.2535

These Components implement the MIFARE NTAG 42xDNA Tag Tamper Protection functions. More...

Collaboration diagram for Commands_TagTamper:

Functions

phStatus_t phalMfNtag42XDna_GetTagTamperStatus (void *pDataParams, uint8_t *pRxBuffer, uint8_t *pRxLen)
 Returns Tag Tamper Status data of the PICC. More...
 

Detailed Description

These Components implement the MIFARE NTAG 42xDNA Tag Tamper Protection functions.

Function Documentation

◆ phalMfNtag42XDna_GetTagTamperStatus()

phStatus_t phalMfNtag42XDna_GetTagTamperStatus ( void *  pDataParams,
uint8_t pRxBuffer,
uint8_t pRxLen 
)

Returns Tag Tamper Status data of the PICC.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[out]pRxBuffer[Out] Read Tag Tamper Protection status
[out]pRxLen[Out] Recieved Length