These Components implement the MIFARE PRIME NTAG Data Management related commands.
More...
|
| phStatus_t | phalMfprimeNtag_ReadData (void *pDataParams, uint8_t bOption, uint8_t bIns, uint8_t bFileNo, uint8_t *pOffset, uint8_t *pLength, uint8_t **ppRxdata, uint16_t *pRxdataLen) |
| | Reads data from standard data files. More...
|
| |
| phStatus_t | phalMfprimeNtag_WriteData (void *pDataParams, uint8_t bOption, uint8_t bIns, uint8_t bFileNo, uint8_t *pOffset, uint8_t *pTxData, uint8_t *pTxDataLen) |
| | Writes data to standard data files. More...
|
| |
These Components implement the MIFARE PRIME NTAG Data Management related commands.
◆ phalMfprimeNtag_ReadData()
Reads data from standard data files.
Chaining upto the size of the HAL Rx buffer is handled within this function. If more data is to be read, the user has to call this function again with bOption = PH_EXCHANGE_RXCHAINING | [one of the communication options]
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bOption | [In] Communication settings for the file.
|
| [in] | bIns | [In] If set, uses ISO 14443-4 chaining instead of DESFire application chaining. |
| [in] | bFileNo | [In] The file number from where the data to be read. |
| [in] | pOffset | [In] The offset from where the data should be read. Will be of 3 bytes with LSB first. If 0x10 need to be offset then it will be 10 00 00. |
| [in] | pLength | [In] The number of bytes to be read. Will be of 3 bytes with LSB first. If 0x10 bytes need to be read then it will be 10 00 00.
If complete file need to be read then it will be 00 00 00. |
| [out] | ppRxdata | [Out] The data retuned by the PICC. |
| [out] | pRxdataLen | [Out] Length of bytes available in RxData buffer. |
◆ phalMfprimeNtag_WriteData()
Writes data to standard data files.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bOption | [In] Communication settings for the file.
|
| [in] | bIns | [In] If set, uses ISO 14443-4 chaining instead of DESFire application chaining. |
| [in] | bFileNo | [In] The file number from where the data to be read. |
| [in] | pOffset | [In] The offset from where the data should be written. Will be of 3 bytes with LSB first. If 0x10 need to be offset then it will be 10 00 00. |
| [in] | pTxData | [In] The data to be written to the PICC. |
| [in] | pTxDataLen | [In] The number of bytes to be written. Will be of 3 bytes with LSB first. If 0x10 bytes need to be written then it will be 10 00 00. |