Data Structures | |
| struct | phalMfPrimeNtag_SamAV3_NonX_DataParams_t |
| MIFARE PRIME NTAG SAM AV3 NonX parameter structure More... | |
Macros | |
| #define | PHAL_MFPRIMENTAG_SAMAV3_NONX_ID 0x02U |
| ID for SamAV3 Non X MIFARE PRIME NTAG layer. | |
Functions | |
| phStatus_t | phalMfPrimeNtag_SamAV3_NonX_Init (phalMfPrimeNtag_SamAV3_NonX_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, phhalHw_SamAV3_DataParams_t *pHalSamDataParams, void *pPalMifareDataParams) |
| Initializes the MIFARE PRIME NTAG Sam AV3 component in Non X mode (S mode). More... | |
| phStatus_t phalMfPrimeNtag_SamAV3_NonX_Init | ( | phalMfPrimeNtag_SamAV3_NonX_DataParams_t * | pDataParams, |
| uint16_t | wSizeOfDataParams, | ||
| phhalHw_SamAV3_DataParams_t * | pHalSamDataParams, | ||
| void * | pPalMifareDataParams | ||
| ) |
Initializes the MIFARE PRIME NTAG Sam AV3 component in Non X mode (S mode).
| PH_ERR_SUCCESS | Operation successful. |
| PH_ERR_INVALID_DATA_PARAMS | for Invaid Dataparams |
| PH_ERR_INVALID_PARAMETER | for invalid parameter values. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | wSizeOfDataParams | [In] Specifies the size of the data parameter structure |
| [in] | pHalSamDataParams | [In] Pointer to the HAL parameter structure of the SAM. |
| [in] | pPalMifareDataParams | [In] Pointer to Pal Mifare parameter structure. |