These Functions implement the MIFARE(R) Classic commands. More...

Modules | |
| Component : Software | |
| Component : Sam_X | |
Macros | |
| #define | PHAL_MFC_VERSION_LENGTH 0x08 |
| Length of a Version MIFARE(R) Classic data block. | |
Functions | |
| phStatus_t | phalMfc_Authenticate (void *pDataParams, uint8_t bBlockNo, uint8_t bKeyType, uint16_t wKeyNumber, uint16_t wKeyVersion, uint8_t *pUid, uint8_t bUidLength) |
| Perform MIFARE(R) Authenticate command with MIFARE Picc. More... | |
| phStatus_t | phalMfc_Read (void *pDataParams, uint8_t bBlockNo, uint8_t *pBlockData) |
| Perform MIFARE(R) Read command with MIFARE Picc. More... | |
| phStatus_t | phalMfc_ReadValue (void *pDataParams, uint8_t bBlockNo, uint8_t *pValue, uint8_t *pAddrData) |
| Perform MIFARE(R) Read Value command with MIFARE Picc. More... | |
| phStatus_t | phalMfc_Write (void *pDataParams, uint8_t bBlockNo, uint8_t *pBlockData) |
| Perform MIFARE(R) Write command with MIFARE Picc. More... | |
| phStatus_t | phalMfc_WriteValue (void *pDataParams, uint8_t bBlockNo, uint8_t *pValue, uint8_t bAddrData) |
| Perform MIFARE(R) Write Value command with MIFARE Picc. More... | |
| phStatus_t | phalMfc_Increment (void *pDataParams, uint8_t bBlockNo, uint8_t *pValue) |
| Perform MIFARE(R) Increment command with MIFARE Picc. More... | |
| phStatus_t | phalMfc_Decrement (void *pDataParams, uint8_t bBlockNo, uint8_t *pValue) |
| Perform MIFARE(R) Decrement command with MIFARE Picc. More... | |
| phStatus_t | phalMfc_Transfer (void *pDataParams, uint8_t bBlockNo) |
| Perform MIFARE(R) Transfer command with MIFARE Picc. More... | |
| phStatus_t | phalMfc_Restore (void *pDataParams, uint8_t bBlockNo) |
| Perform MIFARE(R) Restore command with MIFARE Picc. More... | |
| phStatus_t | phalMfc_IncrementTransfer (void *pDataParams, uint8_t bSrcBlockNo, uint8_t bDstBlockNo, uint8_t *pValue) |
| Perform MIFARE(R) Increment Transfer command sequence with MIFARE Picc. More... | |
| phStatus_t | phalMfc_DecrementTransfer (void *pDataParams, uint8_t bSrcBlockNo, uint8_t bDstBlockNo, uint8_t *pValue) |
| Perform MIFARE(R) Decrement Transfer command sequence with MIFARE Picc. More... | |
| phStatus_t | phalMfc_RestoreTransfer (void *pDataParams, uint8_t bSrcBlockNo, uint8_t bDstBlockNo) |
| Perform MIFARE(R) Restore Transfer command sequence with MIFARE Picc. More... | |
| phStatus_t | phalMfc_PersonalizeUid (void *pDataParams, uint8_t bUidType) |
| Perform MIFARE(R) Personalize UID usage command sequence with MIFARE Picc. More... | |
| phStatus_t | phalMfc_GetVersion (void *pDataParams, uint8_t *pVersion) |
| Perform MIFARE(R) GET VERSION usage command sequence with MIFARE Picc. More... | |
Key section to be used for Authentication form Sectop Trailer. | |
| #define | PHAL_MFC_KEYA 0x0AU |
| MIFARE(R) Key A. | |
| #define | PHAL_MFC_KEYB 0x0BU |
| MIFARE(R) Key B. | |
Block definitions. | |
| #define | PHAL_MFC_DATA_BLOCK_LENGTH 16U |
| Length of a MIFARE(R) Classic data block. | |
| #define | PHAL_MFC_VALUE_BLOCK_LENGTH 4U |
| Length of a MIFARE(R) Classic value block. | |
UID Type definitions. | |
| #define | PHAL_MFC_UID_TYPE_UIDF0 0x00U |
| MIFARE(R) Classic UID type UIDF0. | |
| #define | PHAL_MFC_UID_TYPE_UIDF1 0x40U |
| MIFARE(R) Classic UID type UIDF1. | |
| #define | PHAL_MFC_UID_TYPE_UIDF2 0x20U |
| MIFARE(R) Classic UID type UIDF2. | |
| #define | PHAL_MFC_UID_TYPE_UIDF3 0x60U |
| MIFARE(R) Classic UID type UIDF3. | |
Status Codes of MIFARE(R) Classic PICC. | |
| #define | PHAL_MFC_RESP_ACK 0x0A |
| MIFARE Classic ACK response code. | |
| #define | PHAL_MFC_RESP_NAK0 0x00 |
| MIFARE Classic NAK0 response code. | |
| #define | PHAL_MFC_RESP_NAK1 0x01 |
| MIFARE Classic NAK1 response code. | |
| #define | PHAL_MFC_RESP_NAK4 0x04 |
| MIFARE Classic NAK4 response code. | |
| #define | PHAL_MFC_RESP_NAK5 0x05 |
| MIFARE Classic NAK5 response code. | |
Command Codes of MIFARE(R) Classic PICC. | |
| #define | PHAL_MFC_CMD_RESTORE 0xC2 |
| MIFARE Classic Restore command byte. | |
| #define | PHAL_MFC_CMD_INCREMENT 0xC1 |
| MIFARE Classic Increment command byte. | |
| #define | PHAL_MFC_CMD_DECREMENT 0xC0 |
| MIFARE Classic Decrement command byte. | |
| #define | PHAL_MFC_CMD_TRANSFER 0xB0 |
| MIFARE Classic Transfer command byte. | |
| #define | PHAL_MFC_CMD_READ 0x30 |
| MIFARE Classic Read command byte. | |
| #define | PHAL_MFC_CMD_WRITE 0xA0 |
| MIFARE Classic Write command byte. | |
| #define | PHAL_MFC_CMD_AUTHA 0x60 |
| MIFARE Classic Authenticate A command byte. | |
| #define | PHAL_MFC_CMD_AUTHB 0x61 |
| MIFARE Classic Authenticate B command byte. | |
| #define | PHAL_MFC_CMD_PERSOUID 0x40 |
| MIFARE Classic Personalize UID command. | |
| #define | PHAL_MFC_CMD_GETVERSION 0x62 |
| MIFARE Classic GET VERSION command. | |
These Functions implement the MIFARE(R) Classic commands.
| phStatus_t phalMfc_Authenticate | ( | void * | pDataParams, |
| uint8_t | bBlockNo, | ||
| uint8_t | bKeyType, | ||
| uint16_t | wKeyNumber, | ||
| uint16_t | wKeyVersion, | ||
| uint8_t * | pUid, | ||
| uint8_t | bUidLength | ||
| ) |
Perform MIFARE(R) Authenticate command with MIFARE Picc.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bBlockNo | [In] Blocknumber on card to authenticate to. |
| [in] | bKeyType | [In] The type of key to be used for Authentication. |
| [in] | wKeyNumber | [In] Key number to be used in authentication. |
| [in] | wKeyVersion | [In] Key version to be used in authentication. |
| [in] | pUid | [In] Complete serial number; uint8_t[4/7/10]. |
| [in] | bUidLength | [In] Length of provided serial number (4/7/10). |
| phStatus_t phalMfc_Read | ( | void * | pDataParams, |
| uint8_t | bBlockNo, | ||
| uint8_t * | pBlockData | ||
| ) |
Perform MIFARE(R) Read command with MIFARE Picc.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bBlockNo | [In] Block number to be read. |
| [out] | pBlockData | [Out] pBlockData[16] containing block read from the MIFARE(R) card |
| phStatus_t phalMfc_ReadValue | ( | void * | pDataParams, |
| uint8_t | bBlockNo, | ||
| uint8_t * | pValue, | ||
| uint8_t * | pAddrData | ||
| ) |
Perform MIFARE(R) Read Value command with MIFARE Picc.
| PH_ERR_SUCCESS | Operation successful |
| Other | Depending on implementation and underlaying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bBlockNo | [In] Block number to be read. |
| [out] | pValue | [Out] pValue[4] containing value (LSB first) read from the MIFARE(R) card |
| [out] | pAddrData | [Out] pAddrData containing address read from the MIFARE(R) card value block |
| phStatus_t phalMfc_Write | ( | void * | pDataParams, |
| uint8_t | bBlockNo, | ||
| uint8_t * | pBlockData | ||
| ) |
Perform MIFARE(R) Write command with MIFARE Picc.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bBlockNo | [In] Block number to be written. |
| [in] | pBlockData | [In] pBlockData[16] containing block to be written to the MIFARE(R) card |
| phStatus_t phalMfc_WriteValue | ( | void * | pDataParams, |
| uint8_t | bBlockNo, | ||
| uint8_t * | pValue, | ||
| uint8_t | bAddrData | ||
| ) |
Perform MIFARE(R) Write Value command with MIFARE Picc.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bBlockNo | [In] Block number to be written. |
| [in] | pValue | [In] pValue[4] containing value (LSB first) to be written to the MIFARE(R) card |
| [in] | bAddrData | [In] bAddrData containing address written to the MIFARE(R) card value block |
| phStatus_t phalMfc_Increment | ( | void * | pDataParams, |
| uint8_t | bBlockNo, | ||
| uint8_t * | pValue | ||
| ) |
Perform MIFARE(R) Increment command with MIFARE Picc.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bBlockNo | [In] Block number to be incremented. |
| [in] | pValue | [In] pValue[4] containing value (LSB first) to be incremented on the MIFARE(R) card |
| phStatus_t phalMfc_Decrement | ( | void * | pDataParams, |
| uint8_t | bBlockNo, | ||
| uint8_t * | pValue | ||
| ) |
Perform MIFARE(R) Decrement command with MIFARE Picc.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bBlockNo | [In] Block number to be decremented. |
| [in] | pValue | [In] pValue[4] containing value (LSB first) to be decremented on the MIFARE(R) card |
| phStatus_t phalMfc_Transfer | ( | void * | pDataParams, |
| uint8_t | bBlockNo | ||
| ) |
Perform MIFARE(R) Transfer command with MIFARE Picc.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bBlockNo | [In] Block number the transfer buffer shall be transferred to. |
| phStatus_t phalMfc_Restore | ( | void * | pDataParams, |
| uint8_t | bBlockNo | ||
| ) |
Perform MIFARE(R) Restore command with MIFARE Picc.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bBlockNo | [In] Block number the transfer buffer shall be restored from. |
| phStatus_t phalMfc_IncrementTransfer | ( | void * | pDataParams, |
| uint8_t | bSrcBlockNo, | ||
| uint8_t | bDstBlockNo, | ||
| uint8_t * | pValue | ||
| ) |
Perform MIFARE(R) Increment Transfer command sequence with MIFARE Picc.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bSrcBlockNo | [In] Block number to be incremented. |
| [in] | bDstBlockNo | [In] Block number to be transferred to. |
| [in] | pValue | [In] pValue[4] containing value (LSB first) to be incremented on the MIFARE(R) card |
| phStatus_t phalMfc_DecrementTransfer | ( | void * | pDataParams, |
| uint8_t | bSrcBlockNo, | ||
| uint8_t | bDstBlockNo, | ||
| uint8_t * | pValue | ||
| ) |
Perform MIFARE(R) Decrement Transfer command sequence with MIFARE Picc.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bSrcBlockNo | [In] Block number to be decremented. |
| [in] | bDstBlockNo | [In] Block number to be transferred to. |
| [in] | pValue | [In] pValue[4] containing value (LSB first) to be decremented on the MIFARE(R) card. |
| phStatus_t phalMfc_RestoreTransfer | ( | void * | pDataParams, |
| uint8_t | bSrcBlockNo, | ||
| uint8_t | bDstBlockNo | ||
| ) |
Perform MIFARE(R) Restore Transfer command sequence with MIFARE Picc.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bSrcBlockNo | [In] block number to be decremented. |
| [in] | bDstBlockNo | [In] block number to be transferred to. |
| phStatus_t phalMfc_PersonalizeUid | ( | void * | pDataParams, |
| uint8_t | bUidType | ||
| ) |
Perform MIFARE(R) Personalize UID usage command sequence with MIFARE Picc.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bUidType | [In] UID type. One of the below Types. |
| phStatus_t phalMfc_GetVersion | ( | void * | pDataParams, |
| uint8_t * | pVersion | ||
| ) |
Perform MIFARE(R) GET VERSION usage command sequence with MIFARE Picc.
GET_VERSION command is used to retrieve information about the NTAG family, the product version, storage size and other product data required to identify the specific NTAG-I2C return Status code
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [out] | pVersion | [Out] Version returned by PICC. |