NXP Reader Library  v17.1.0.2535
MIFARE DESFire EVx

These Functions implement the MIFARE DESFire EVx commands. More...

Collaboration diagram for MIFARE DESFire EVx:

Modules

 Component : Software
 
 Component : Sam_NonX
 
 Component : Sam_X
 
 Commands_SecureMessaging
 These Components implement the MIFARE DESFire EVx Secure Messaging related commands.
 
 Commands_MemoryConfiguration
 These Components implement the MIFARE DESFire EVx Memory and Configuration Management related commands.
 
 Commands_KeyManagement
 These Components implement the MIFARE DESFire EVx Key Management related commands.
 
 Commands_ApplicationManagement
 These Components implement the MIFARE DESFire EVx Application Management related commands.
 
 Commands_FileManagement
 These Components implement the MIFARE DESFire EVx File Management related commands.
 
 Commands_DataManagement
 These Components implement the MIFARE DESFire EVx Data Management related commands.
 
 Commands_TransactionManagement
 These Components implement the MIFARE DESFire EVx Transaction Management related commands.
 
 Commands_ISO7816
 These Components implement the MIFARE DESFire EVx ISO/IEC 7816-4 Basic commands.
 
 Commands_OriginalityCheck
 These Components implement the MIFARE DESFire EVx Originality Check functions.
 
 Commands_MIFARE_ClassicSupport
 These Components implement the MIFARE DESFire EVx MIFARE Classic Support functions.
 
 Commands_PostDeliveryConfiguration
 These Components implement the MIFARE DESFire EVx MIFARE Post Delivery configuration function.
 
 Commands_Miscellaneous
 These Components implement the MIFARE DESFire EVx Miscellaneous functions. These are not part of actual DESFire EVx data sheet rather its for internal purpose.
 

Other Options for various Functions

#define PHAL_MFDFEVX_ORIGINALITY_KEY_FIRST   0x01U
 Originality key for AES.
 
#define PHAL_MFDFEVX_ORIGINALITY_KEY_LAST   0x04U
 Originality key for AES

 
#define PHAL_MFDFEVX_MAC_DATA_INCOMPLETE   0x01U
 Option for indicating more data to come in next call for MAC calculation.
 
#define PHAL_MFDFEVX_COMMUNICATION_MAC_ON_RC   0x02U
 MAC is appended over response

 
#define PHAL_MFDFEVX_COMMUNICATION_MAC_ON_CMD   0x03U
 MAC is appended over command.
 
#define PHAL_MFDFEVX_AUTHENTICATE_RESET   0x08U
 authentication state shall be reset
 
#define PHAL_MFDFEVX_KEYSETVALUES_PRESENT   0x01U
 Bit 0 of bKeySettings3 decides the presence of the key set values array.
 
#define PHAL_MFDFEVX_KEYSETT3_PRESENT   0x10U
 Bit 4 of bKeySettings2 decides the presence of the keysetting3.
 
#define PHAL_MFDFEVX_MFC_KILL_KEY   0x31U
 MFCKill key for AES.
 

Error Codes mapping to custom values.

#define PHAL_MFDFEVX_NO_CHANGES   (PH_ERR_CUSTOM_BEGIN + 0)
 MFDFEVx Response - No changes done to backup files.
 
#define PHAL_MFDFEVX_ERR_OUT_OF_EEPROM_ERROR   (PH_ERR_CUSTOM_BEGIN + 1)
 MFDFEVx Response - Insufficient NV-Memory.
 
#define PHAL_MFDFEVX_ERR_NO_SUCH_KEY   (PH_ERR_CUSTOM_BEGIN + 2)
 MFDFEVx Invalid key number specified.
 
#define PHAL_MFDFEVX_ERR_PERMISSION_DENIED   (PH_ERR_CUSTOM_BEGIN + 3)
 MFDFEVx Current configuration/status does not allow the requested command.
 
#define PHAL_MFDFEVX_ERR_APPLICATION_NOT_FOUND   (PH_ERR_CUSTOM_BEGIN + 4)
 MFDFEVx Requested AID not found on PICC.
 
#define PHAL_MFDFEVX_ERR_BOUNDARY_ERROR   (PH_ERR_CUSTOM_BEGIN + 5)
 MFDFEVx Attempt to read/write data from/to beyond the files/record's limits.
 
#define PHAL_MFDFEVX_ERR_COMMAND_ABORTED   (PH_ERR_CUSTOM_BEGIN + 6)
 MFDFEVx Previous cmd not fully completed. More...
 
#define PHAL_MFDFEVX_ERR_COUNT   (PH_ERR_CUSTOM_BEGIN + 7)
 MFDFEVx Num. More...
 
#define PHAL_MFDFEVX_ERR_DUPLICATE   (PH_ERR_CUSTOM_BEGIN + 8)
 MFDFEVx File/Application with same number already exists.
 
#define PHAL_MFDFEVX_ERR_FILE_NOT_FOUND   (PH_ERR_CUSTOM_BEGIN + 9)
 MFDFEVx Specified file number does not exist.
 
#define PHAL_MFDFEVX_ERR_PICC_CRYPTO   (PH_ERR_CUSTOM_BEGIN + 10)
 MFDFEVx Crypto error returned by PICC.
 
#define PHAL_MFDFEVX_ERR_PARAMETER_ERROR   (PH_ERR_CUSTOM_BEGIN + 11)
 MFDFEVx Parameter value error returned by PICC.
 
#define PHAL_MFDFEVX_ERR_DF_GEN_ERROR   (PH_ERR_CUSTOM_BEGIN + 12)
 MFDFEVx DesFire Generic error. More...
 
#define PHAL_MFDFEVX_ERR_DF_7816_GEN_ERROR   (PH_ERR_CUSTOM_BEGIN + 13)
 MFDFEVx ISO 7816 Generic error. More...
 
#define PHAL_MFDFEVX_ERR_CMD_INVALID   (PH_ERR_CUSTOM_BEGIN + 14)
 MFDFEVx ISO 7816 Generic error. More...
 
#define PHAL_MFDFEVX_ERR_NOT_SUPPORTED   (PH_ERR_CUSTOM_BEGIN + 15)
 MFDFEVx Not Supported Error.
 
#define PHAL_MFDFEVX_ERR_INTEGRITY_ERROR   (PH_ERR_CUSTOM_BEGIN + 16)
 MFDFEVx integrity error.
 
#define PHAL_MFDFEVX_ERR_MEMORY_ERROR   (PH_ERR_CUSTOM_BEGIN + 17)
 MFDFEVx memory error.
 
#define PHAL_MFDFEVX_ERR_OPERATION_OK_LIM   (PH_ERR_CUSTOM_BEGIN + 27)
 MFDFEVx custom error code for Successful operation with limited functionality.
 
#define PHAL_MFDFEVX_ERR_CMD_OVERFLOW   (PH_ERR_CUSTOM_BEGIN + 28)
 MFDFEVx Too many commands in the session or transaction.
 
#define PHAL_MFDFEVX_ERR_GEN_FAILURE   (PH_ERR_CUSTOM_BEGIN + 29)
 MFDFEVx Failure in the operation of the PD.
 
#define PHAL_MFDFEVX_ERR_BNR   (PH_ERR_CUSTOM_BEGIN + 30)
 MFDFEVx Invalid Block number: not existing in the implementation or not valid to target with this command.
 
#define PHAL_MFDFEVX_ERR_FORMAT   (PH_ERR_CUSTOM_BEGIN + 31)
 MFDFEVx Format of the command is not correct (e.g. More...
 

ISO7816-4 Error Codes mapping to custom values.

#define PHAL_MFDFEVX_ISO7816_CUSTOM_ERR_MEMORY_FAILURE   (PH_ERR_CUSTOM_BEGIN + 18)
 ISO7816 custom response code for memory failure.
 
#define PHAL_MFDFEVX_ISO7816_CUSTOM_ERR_WRONG_LENGTH   (PH_ERR_CUSTOM_BEGIN + 19)
 ISO7816 custom response code for wrong length, no further indication.
 
#define PHAL_MFDFEVX_ISO7816_CUSTOM_ERR_SECURITY_STAT_NOT_SATISFIED   (PH_ERR_CUSTOM_BEGIN + 20)
 ISO7816 custom response code for security status not satisfied.
 
#define PHAL_MFDFEVX_ISO7816_CUSTOM_ERR_CONDITIONS_NOT_SATISFIED   (PH_ERR_CUSTOM_BEGIN + 21)
 ISO7816 custom response code for conditions of use not satisfied.
 
#define PHAL_MFDFEVX_ISO7816_CUSTOM_ERR_FILE_APPLICATION_NOT_FOUND   (PH_ERR_CUSTOM_BEGIN + 22)
 ISO7816 custom response code for file or application not found.
 
#define PHAL_MFDFEVX_ISO7816_CUSTOM_ERR_INCORRECT_PARAM_P1_P2   (PH_ERR_CUSTOM_BEGIN + 23)
 ISO7816 custom response code for incorrect parameters P1-P2.
 
#define PHAL_MFDFEVX_ISO7816_CUSTOM_ERR_LC_INCONSISTENT   (PH_ERR_CUSTOM_BEGIN + 24)
 ISO7816 custom response code for LC inconsistent with parameter P1-P2.
 
#define PHAL_MFDFEVX_ISO7816_CUSTOM_ERR_WRONG_LE   (PH_ERR_CUSTOM_BEGIN + 25)
 ISO7816 custom response code for wrong LE field.
 
#define PHAL_MFDFEVX_ISO7816_CUSTOM_ERR_INS_CODE_NOT_SUPPORTED   (PH_ERR_CUSTOM_BEGIN + 26)
 ISO7816 custom response code for instruction code not supported or invalid.
 

Authentication Modes

#define PHAL_MFDFEVX_NOT_AUTHENTICATED   0xFFU
 No authentication.
 
#define PHAL_MFDFEVX_AUTHENTICATE   0x0AU
 D40 Authentication; 0x0A.
 
#define PHAL_MFDFEVX_AUTHENTICATEISO   0x1AU
 ISO Authentication; 0x1A.
 
#define PHAL_MFDFEVX_AUTHENTICATEAES   0xAAU
 AES Authentication; 0xAA.
 
#define PHAL_MFDFEVX_AUTHENTICATEEV2   0x71U
 EV2 Authentication; 0x71.
 
#define PHAL_MFDFEVX_AUTH_FIRST   0x01U
 Option to perform EVx First Authentication.
 
#define PHAL_MFDFEVX_AUTH_NONFIRST   0x00U
 Option to perform EVx NonFirst Authentication.
 

Option to be used for InitializeKeySet and CreateTransactionMACFile command.

#define PHAL_MFDFEVX_KEY_TYPE_2K3DES   0x00U
 Option for 2 Key Triple Des key type.
 
#define PHAL_MFDFEVX_KEY_TYPE_3K3DES   0x01U
 Option for 3 Key Triple Des key type.
 
#define PHAL_MFDFEVX_KEY_TYPE_AES128   0x02U
 Option for AES 128 key type.
 

Option for most of the commands.

#define PHAL_MFDFEVX_SAI   0x80U
 Option for Secondary application indicator (SAI).
 

Options for application / file creation commands command.

#define PHAL_MFDFEVX_ISO_FILE_INFO_NOT_AVAILABLE   0x00U
 Option to indicate no ISO File ID or ISODFName are present.
 
#define PHAL_MFDFEVX_ISO_FILE_ID_AVAILABLE   0x01U
 Option to indicate the presence of ISO FileID.
 
#define PHAL_MFDFEVX_ISO_DF_NAME_AVAILABLE   0x02U
 Option to indicate the presence of ISO DFName.
 
#define PHAL_MFDFEVX_ISO_FILE_ID_DF_NAME_AVAILABLE   0x03U
 Option to indicate the presence of both ISO FileID and ISO DFName.
 

The communication mode to be used.

#define PHAL_MFDFEVX_COMMUNICATION_PLAIN   0x00U
 Plain mode of communication.
 
#define PHAL_MFDFEVX_COMMUNICATION_PLAIN_1   0x20U
 Plain mode of communication.
 
#define PHAL_MFDFEVX_COMMUNICATION_MACD   0x10U
 MAC mode of communication.
 
#define PHAL_MFDFEVX_COMMUNICATION_ENC   0x30U
 Enciphered mode of communication.
 

Detailed Description

These Functions implement the MIFARE DESFire EVx commands.

Macro Definition Documentation

◆ PHAL_MFDFEVX_ERR_COMMAND_ABORTED

#define PHAL_MFDFEVX_ERR_COMMAND_ABORTED   (PH_ERR_CUSTOM_BEGIN + 6)

MFDFEVx Previous cmd not fully completed.

Not all frames were requested or provided by the PCD.

◆ PHAL_MFDFEVX_ERR_COUNT

#define PHAL_MFDFEVX_ERR_COUNT   (PH_ERR_CUSTOM_BEGIN + 7)

MFDFEVx Num.

of applns limited to 28. No additional applications possible.

◆ PHAL_MFDFEVX_ERR_DF_GEN_ERROR

#define PHAL_MFDFEVX_ERR_DF_GEN_ERROR   (PH_ERR_CUSTOM_BEGIN + 12)

MFDFEVx DesFire Generic error.

Check additional Info.

◆ PHAL_MFDFEVX_ERR_DF_7816_GEN_ERROR

#define PHAL_MFDFEVX_ERR_DF_7816_GEN_ERROR   (PH_ERR_CUSTOM_BEGIN + 13)

MFDFEVx ISO 7816 Generic error.

Check Additional Info.

◆ PHAL_MFDFEVX_ERR_CMD_INVALID

#define PHAL_MFDFEVX_ERR_CMD_INVALID   (PH_ERR_CUSTOM_BEGIN + 14)

MFDFEVx ISO 7816 Generic error.

Check Additional Info.

◆ PHAL_MFDFEVX_ERR_FORMAT

#define PHAL_MFDFEVX_ERR_FORMAT   (PH_ERR_CUSTOM_BEGIN + 31)

MFDFEVx Format of the command is not correct (e.g.

too many or too few bytes).