These Components implement the MIFARE DESFire EVx Application Management related commands.
More...
|
| phStatus_t | phalMfdfEVx_CreateApplication (void *pDataParams, uint8_t bOption, uint8_t *pAid, uint8_t bKeySettings1, uint8_t bKeySettings2, uint8_t bKeySettings3, uint8_t *pKeySetValues, uint8_t *pISOFileId, uint8_t *pISODFName, uint8_t bISODFNameLen) |
| | Creates new applications on the PICC. More...
|
| |
| phStatus_t | phalMfdfEVx_DeleteApplication (void *pDataParams, uint8_t *pAid, uint8_t *pDAMMAC, uint8_t bDAMMAC_Len) |
| | Permanently deletes the applications on the PICC. More...
|
| |
| phStatus_t | phalMfdfEVx_CreateDelegatedApplication (void *pDataParams, uint8_t bOption, uint8_t *pAid, uint8_t *pDamParams, uint8_t bKeySettings1, uint8_t bKeySettings2, uint8_t bKeySettings3, uint8_t *pKeySetValues, uint8_t *pISOFileId, uint8_t *pISODFName, uint8_t bISODFNameLen, uint8_t *pEncK, uint8_t *pDAMMAC) |
| | Creates new Delegated application For delegated application creation, the PICC level (AID 0x000000) must have been selected. More...
|
| |
| phStatus_t | phalMfdfEVx_SelectApplication (void *pDataParams, uint8_t bOption, uint8_t *pAid, uint8_t *pAid2) |
| | Selects one particular application on the PICC for further access. More...
|
| |
| phStatus_t | phalMfdfEVx_GetApplicationIDs (void *pDataParams, uint8_t bOption, uint8_t **pAidBuff, uint8_t *pNumAid) |
| | Returns application identifiers of all applications on the PICC. More...
|
| |
| phStatus_t | phalMfdfEVx_GetDFNames (void *pDataParams, uint8_t bOption, uint8_t *pDFBuffer, uint8_t *bDFInfoLen) |
| | Returns the Dedicated File(DF) names. More...
|
| |
| phStatus_t | phalMfdfEVx_GetDelegatedInfo (void *pDataParams, uint8_t *pDAMSlot, uint8_t *pDamSlotVer, uint8_t *pQuotaLimit, uint8_t *pFreeBlocks, uint8_t *pAid) |
| | Parameters associated with the delegated application can be retrieved using this command. More...
|
| |
These Components implement the MIFARE DESFire EVx Application Management related commands.
◆ phalMfdfEVx_CreateApplication()
Creates new applications on the PICC.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bOption | [In] Option to represent the present of ISO information.
|
| [in] | pAid | [In] The application identifier to be used. Will be of 3 bytes with LSB first. If application 01 need to be created then the Aid will be 01 00 00. |
| [in] | bKeySettings1 | [In] Application Key settings. |
| [in] | bKeySettings2 | [In] Additional key settings. |
| [in] | bKeySettings3 | [In] Additional key settings. |
| [in] | pKeySetValues | [In] The Key set values for the application. Should as mentioned below.
Byte0 = AKS Ver
Byte1 = Number of KeySets
Byte2 = MaxKeysize
Byte3 = Application KeySet Settings. |
| [in] | pISOFileId | [In] ISO File ID to be used. Will be two bytes. |
| [in] | pISODFName | [In] ISO DF Name to be used. Will be 16 bytes and can also be NULL based on the option. |
| [in] | bISODFNameLen | [In] Length of bytes available in ISODFName buffer. |
◆ phalMfdfEVx_DeleteApplication()
Permanently deletes the applications on the PICC.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | pAid | [In] The application identifier to be used. Will be of 3 bytes with LSB first.
If application 01 need to be deleted then the Aid will be 01 00 00. |
| [in] | pDAMMAC | [In] [Optional, present if PICCDAMAuthKey or NXPDAMAuthKey is used for authentication] The MAC calculated by the card issuer to allow delegated application deletion. |
| [in] | bDAMMAC_Len | [In] Length of bytes available in DAMMAC buffer. |
◆ phalMfdfEVx_CreateDelegatedApplication()
| phStatus_t phalMfdfEVx_CreateDelegatedApplication |
( |
void * |
pDataParams, |
|
|
uint8_t |
bOption, |
|
|
uint8_t * |
pAid, |
|
|
uint8_t * |
pDamParams, |
|
|
uint8_t |
bKeySettings1, |
|
|
uint8_t |
bKeySettings2, |
|
|
uint8_t |
bKeySettings3, |
|
|
uint8_t * |
pKeySetValues, |
|
|
uint8_t * |
pISOFileId, |
|
|
uint8_t * |
pISODFName, |
|
|
uint8_t |
bISODFNameLen, |
|
|
uint8_t * |
pEncK, |
|
|
uint8_t * |
pDAMMAC |
|
) |
| |
Creates new Delegated application For delegated application creation, the PICC level (AID 0x000000) must have been selected.
An active authentication with the PICCDAMAuthKey is required.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bOption | [In] Option to represent the present of ISO information.
|
| [in] | pAid | [In] The application identifier to be used. Will be of 3 bytes with LSB first. If application 01 need to be created then the Aid will be 01 00 00. |
| [in] | pDamParams | [In] The DAM information. Should as mentioned below.
Byte0 = DAM Slot No [LSB]
Byte1 = DAM Slot No [MSB]
Byte2 = DAM Slot Version
Byte3 = Quota Limit [LSB]
Byte4 = Quota Limit [MSB] |
| [in] | bKeySettings1 | [In] Application Key settings. |
| [in] | bKeySettings2 | [In] Additional key settings. |
| [in] | bKeySettings3 | [In] Additional key settings. |
| [in] | pKeySetValues | [In] The Key set values for the application. Should as mentioned below.
Byte0 = AKS ver
Byte1 = Number of KeySets
Byte2 = MaxKeysize
Byte3 = Application KeySet Settings. |
| [in] | pISOFileId | [In] ISO File ID to be used. Will be two bytes. |
| [in] | pISODFName | [In] ISO DF Name to be used. Will be 16 bytes and can also be NULL based on the option. |
| [in] | bISODFNameLen | [In] Length of bytes available in ISODFName buffer. |
| [in] | pEncK | [In] Encrypted initial application key. 32 bytes long. |
| [in] | pDAMMAC | [In] 8 byte DAM MAC. |
◆ phalMfdfEVx_SelectApplication()
Selects one particular application on the PICC for further access.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bOption | [In] One of the below options.
|
| [in] | pAid | [In] The primary application identifier to be used. Will be of 3 bytes with LSB first. If application 01 need to be selected then the Aid will be 01 00 00. |
| [in] | pAid2 | [In] The secondary application identifier to be used. Will be of 3 bytes with LSB first. If application 01 need to be selected then the Aid will be 01 00 00. |
◆ phalMfdfEVx_GetApplicationIDs()
Returns application identifiers of all applications on the PICC.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bOption | [In] One of the below options.
|
| [out] | pAidBuff | [Out] The available identifiers of the application(s). |
| [out] | pNumAid | [Out] The number of available application(s). |
◆ phalMfdfEVx_GetDFNames()
Returns the Dedicated File(DF) names.
CAUTION: This should not be called with AES or ISO authentication DOING SO WILL DAMAGE THE DESFIRE Card
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bOption | [In] One of the below options.
|
| [out] | pDFBuffer | [Out] The ISO information about the application. At a time the information of one application will be returned. The buffer should be 21 (3 + 2 + 16) bytes long. |
| [out] | bDFInfoLen | [Out] Length of bytes available in DFBuffer buffer. |
◆ phalMfdfEVx_GetDelegatedInfo()
Parameters associated with the delegated application can be retrieved using this command.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | pDAMSlot | [In] Slot number associated with the memory space of the targeted delegated application. LSB first. |
| [out] | pDamSlotVer | [Out] Slot version associated with the memory space of the targeted delegated application. |
| [out] | pQuotaLimit | [Out] Maximal memory consumption of the targeted delegated application (in 32-byte blocks). |
| [out] | pFreeBlocks | [Out] Amount of unallocated memory of the targeted delegated application (in 32-byte blocks). |
| [out] | pAid | [Out] Application Identifier of the targeted DAM slot. This parameter is set to 0x000000 if the DAM slot targeted by DAMSlotNo exists on the card, but is currently not occupied with an application, i.e. the latest application has been deleted. |