These Components implement the MIFARE DESFire EVx Miscellaneous functions. These are not part of actual DESFire EVx data sheet rather its for internal purpose. More...

Functions | |
| phStatus_t | phalMfdfEVx_GetConfig (void *pDataParams, uint16_t wConfig, uint16_t *pValue) |
| Perform a GetConfig command. More... | |
| phStatus_t | phalMfdfEVx_SetConfig (void *pDataParams, uint16_t wConfig, uint16_t wValue) |
| Perform a SetConfig command. More... | |
| phStatus_t | phalMfdfEVx_ResetAuthentication (void *pDataParams) |
| Reset the authentication. More... | |
| phStatus_t | phalMfdfEVx_GenerateDAMEncKey (void *pDataParams, uint16_t wKeyNoDAMEnc, uint16_t wKeyVerDAMEnc, uint16_t wKeyNoAppDAMDefault, uint16_t wKeyVerAppDAMDefault, uint8_t bAppDAMDefaultKeyVer, uint8_t *pDAMEncKey) |
| Generates Encrypted Key for Delegated application management. More... | |
| phStatus_t | phalMfdfEVx_GenerateDAMMAC (void *pDataParams, uint8_t bOption, uint16_t wKeyNoDAMMAC, uint16_t wKeyVerDAMMAC, uint8_t *pAid, uint8_t *pDamParams, uint8_t bKeySettings1, uint8_t bKeySettings2, uint8_t bKeySettings3, uint8_t *pKeySetValues, uint8_t *pISOFileId, uint8_t *pISODFName, uint8_t bISODFNameLen, uint8_t *pEncK, uint8_t *pDAMMAC) |
| Generate MAC for Delegated application management. More... | |
| phStatus_t | phalMfdfEVx_GenerateDAMMACSetConfig (void *pDataParams, uint16_t wKeyNoDAMMAC, uint16_t wKeyVerDAMMAC, uint16_t wOldDFNameLen, uint8_t *pOldISODFName, uint16_t wNewDFNameLen, uint8_t *pNewISODFName, uint8_t *pDAMMAC) |
| Generates DAMMAC for Set Configuration with option 0x06 for Delegated Application. More... | |
| phStatus_t | phalMfdfEVx_CalculateTMV (void *pDataParams, uint16_t wOption, uint16_t wKeyNoTMACKey, uint16_t wKeyVerTMACKey, uint16_t wRamKeyNo, uint16_t wRamKeyVer, uint8_t *pDivInput, uint8_t bDivInputLen, uint8_t *pTMC, uint8_t *pUid, uint8_t bUidLen, uint8_t *pTMI, uint32_t dwTMILen, uint8_t *pTMV) |
| Computed the Transaction MAC input as performed on the PICC. More... | |
| phStatus_t | phalMfdfEVx_DecryptReaderID (void *pDataParams, uint16_t wOption, uint16_t wKeyNoTMACKey, uint16_t wKeyVerTMACKey, uint16_t wRamKeyNo, uint16_t wRamKeyVer, uint8_t *pDivInput, uint8_t bDivInputLen, uint8_t *pTMC, uint8_t *pUid, uint8_t bUidLen, uint8_t *pEncTMRI, uint8_t *pTMRIPrev) |
| Decrypted the reader ID as performed on the PICC. More... | |
| phStatus_t | phalMfdfEVx_ComputeMFCLicenseMAC (void *pDataParams, uint16_t wOption, uint16_t wMFCLicenseMACKeyNo, uint16_t wMFCLicenseMACKeyVer, uint8_t *pInput, uint16_t wInputLen, uint8_t *pDivInput, uint8_t bDivInputLen, uint8_t *pMFCLicenseMAC) |
| Compute the MFCLicenseMAC for phalMfdfEVx_CreateMFCMapping and phalMfdfEVx_RestrictMFCUpdate command. More... | |
| phStatus_t | phalMfdfEVx_CalculateMACSDM (void *pDataParams, uint8_t bSdmOption, uint16_t wSDMMacKeyNo, uint16_t wSDMMacKeyVer, uint16_t wRamKeyNo, uint16_t wRamKeyVer, uint8_t *pUid, uint8_t bUidLen, uint8_t *SDMReadCtr, uint8_t *pInData, uint16_t wInDataLen, uint8_t *pRespMac) |
Calculate MAC SDM While using this command in SAM mode make sure the below points are taken careSDMMacKeyNo and RamKeyNo should be off Offline_Crypto Keyclass. More... | |
| phStatus_t | phalMfdfEVx_DecryptSDMENCFileData (void *pDataParams, uint8_t bSdmOption, uint16_t wEncKeyNo, uint16_t wEncKeyVer, uint16_t wRamKeyNo, uint16_t wRamKeyVer, uint8_t *pUid, uint8_t bUidLen, uint8_t *pSDMReadCtr, uint8_t *pEncdata, uint16_t wInDataLen, uint8_t *pPlainData) |
| Decrypt SDM enciphered data. More... | |
| phStatus_t | phalMfdfEVx_DecryptSDMPICCData (void *pDataParams, uint16_t wKeyNo, uint16_t wKeyVer, uint8_t *pEncdata, uint16_t wInDataLen, uint8_t *pPlainData) |
| Decrypt SDM PICC Data. More... | |
| phStatus_t | phalMfdfEVx_SetVCAParams (void *pDataParams, void *pAlVCADataParams) |
| This is a utility API which sets the VCA structure in DESFire EVx structure params. More... | |
Options to diversify the key. | |
| #define | PHAL_MFDFEVX_DIVERSIFICATION_OFF 0xFFFFU |
| Option to disable key diversification. | |
| #define | PHAL_MFDFEVX_DIVERSIFICATION_ON 0x0000U |
| Option to enable key diversification. | |
The configuration to be used for SetConfig / GetConfig. | |
| #define | PHAL_MFDFEVX_ADDITIONAL_INFO 0x00A1 |
| Option for GetConfig/SetConfig to get/set additional info of a generic error or some length exposed by interfaces. | |
| #define | PHAL_MFDFEVX_WRAPPED_MODE 0x00A2 |
| Option for GetConfig/SetConfig to get/set current status of command wrapping in ISO 7816-4 APDUs. | |
| #define | PHAL_MFDFEVX_SHORT_LENGTH_APDU 0x00A3 |
| Option for GetConfig/SetConfig to get/set current status of Short Length APDU wrapping in ISO 7816-4 APDUs. | |
| #define | PHAL_MFDFEVX_RETURN_FAB_ID 0x00A4 |
| Option for GetConfig/SetConfig to get/set Fabrication Identifier of the product. More... | |
The options to be used for GenerateDAMMAC. | |
| #define | PHAL_MFDFEVX_GENERATE_DAMMAC_CREATE_APPLICATION 0x00 |
| Option to indicate the DAMMAC generation is for phalMfdfEVx_CreateDelegatedApplication command. | |
| #define | PHAL_MFDFEVX_GENERATE_DAMMAC_DELETE_APPLICATION 0x80 |
| Option to indicate the DAMMAC generation is for phalMfdfEVx_DeleteApplication command. | |
Options for SDM information. | |
| #define | PHAL_MFDFEVX_VCUID_PRESENT 0x80U |
| Only VCUID is considred for SDM Session key calculation. | |
| #define | PHAL_MFDFEVX_RDCTR_PRESENT 0x40U |
| Only RDCTR is considred for SDM Session key calculation. | |
These Components implement the MIFARE DESFire EVx Miscellaneous functions. These are not part of actual DESFire EVx data sheet rather its for internal purpose.
| #define PHAL_MFDFEVX_RETURN_FAB_ID 0x00A4 |
Option for GetConfig/SetConfig to get/set Fabrication Identifier of the product.
This will be utilized while performing GetVersion command.
| phStatus_t phalMfdfEVx_GetConfig | ( | void * | pDataParams, |
| uint16_t | wConfig, | ||
| uint16_t * | pValue | ||
| ) |
Perform a GetConfig command.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | wConfig | [In] Configuration to read. Will be one of the below values. |
| [out] | pValue | [Out] The value for the mentioned configuration. |
| phStatus_t phalMfdfEVx_SetConfig | ( | void * | pDataParams, |
| uint16_t | wConfig, | ||
| uint16_t | wValue | ||
| ) |
Perform a SetConfig command.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | wConfig | [In] Configuration to set. Will be one of the below values. |
| [in] | wValue | [In] The value for the mentioned configuration. |
| phStatus_t phalMfdfEVx_ResetAuthentication | ( | void * | pDataParams | ) |
Reset the authentication.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| phStatus_t phalMfdfEVx_GenerateDAMEncKey | ( | void * | pDataParams, |
| uint16_t | wKeyNoDAMEnc, | ||
| uint16_t | wKeyVerDAMEnc, | ||
| uint16_t | wKeyNoAppDAMDefault, | ||
| uint16_t | wKeyVerAppDAMDefault, | ||
| uint8_t | bAppDAMDefaultKeyVer, | ||
| uint8_t * | pDAMEncKey | ||
| ) |
Generates Encrypted Key for Delegated application management.
While using this command in SAM mode make sure the below points are taken care
KeyNoAppDAMDefault should have AllowDumpSecretKey enabled.
KeyNoDAMEnc should be off Offline_Crypto Keyclass.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | [In] Pointer to this layers parameter structure. |
| [in] | wKeyNoDAMEnc | [In] Key number in key store of DAM Encryption key. |
| [in] | wKeyVerDAMEnc | [In] Key version in key store of DAM Encryption key. |
| [in] | wKeyNoAppDAMDefault | [In] Key number in key store of DAM default key. |
| [in] | wKeyVerAppDAMDefault | [In] Key version in key store of DAM default key. |
| [in] | bAppDAMDefaultKeyVer | [In] DAM Default Key version. Value should be valid for AES key. Ignored for other key types. |
| [out] | pDAMEncKey | [Out] Encrypted DAM Default key data. |
| phStatus_t phalMfdfEVx_GenerateDAMMAC | ( | void * | pDataParams, |
| uint8_t | bOption, | ||
| uint16_t | wKeyNoDAMMAC, | ||
| uint16_t | wKeyVerDAMMAC, | ||
| uint8_t * | pAid, | ||
| uint8_t * | pDamParams, | ||
| uint8_t | bKeySettings1, | ||
| uint8_t | bKeySettings2, | ||
| uint8_t | bKeySettings3, | ||
| uint8_t * | pKeySetValues, | ||
| uint8_t * | pISOFileId, | ||
| uint8_t * | pISODFName, | ||
| uint8_t | bISODFNameLen, | ||
| uint8_t * | pEncK, | ||
| uint8_t * | pDAMMAC | ||
| ) |
Generate MAC for Delegated application management.
While using this command in SAM mode make sure the below points are taken care
KeyNoDAMMAC should be off Offline_Crypto KeyClass.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | [In] Pointer to this layers parameter structure. |
| [in] | bOption | [In] Option to represent the present of ISO information. |
| [in] | wKeyNoDAMMAC | [In] Key number in key store of DAM MAC key. |
| [in] | wKeyVerDAMMAC | [In] Key version in key store of DAM MAC key. |
| [in] | pAid | [In] The application identifier to be used. Will be of 3 bytes with LSB first. If application 01 need to be created then the Aid will be 01 00 00. |
| [in] | pDamParams | [In] The DAM information. Should as mentioned below.Byte0 = DAM Slot No [LSB]Byte1 = DAM Slot No [MSB]Byte2 = DAM Slot VersionByte3 = Quota Limit [LSB]Byte4 = Quota Limit [MSB] |
| [in] | bKeySettings1 | [In] Application Key settings. |
| [in] | bKeySettings2 | [In] Additional key settings. |
| [in] | bKeySettings3 | [In] Additional key settings. |
| [in] | pKeySetValues | [In] The Key set values for the application. Should as mentioned below.Byte0 = AKS verByte1 = Number of KeySetsByte2 = MaxKeysizeByte3 = Application KeySet Settings. |
| [in] | pISOFileId | [In] ISO File ID to be used. Will be two bytes. |
| [in] | pISODFName | [In] ISO DF Name to be used. Will be 16 bytes and can also be NULL based on the option. |
| [in] | bISODFNameLen | [In] Length of bytes available in ISODFName buffer. |
| [in] | pEncK | [In] Encrypted initial application key. 32 bytes long. |
| [out] | pDAMMAC | [Out] 8 byte DAMMAC. |
| phStatus_t phalMfdfEVx_GenerateDAMMACSetConfig | ( | void * | pDataParams, |
| uint16_t | wKeyNoDAMMAC, | ||
| uint16_t | wKeyVerDAMMAC, | ||
| uint16_t | wOldDFNameLen, | ||
| uint8_t * | pOldISODFName, | ||
| uint16_t | wNewDFNameLen, | ||
| uint8_t * | pNewISODFName, | ||
| uint8_t * | pDAMMAC | ||
| ) |
Generates DAMMAC for Set Configuration with option 0x06 for Delegated Application.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | [In] Pointer to this layers parameter structure. |
| [in] | wKeyNoDAMMAC | [In] Key number in key store of DAM MAC Key |
| [in] | wKeyVerDAMMAC | [In] Key version in key store of DAM MAC Key |
| [in] | wOldDFNameLen | [In] Length of existing DF Name |
| [in] | pOldISODFName | [In] This means already created delegated app ISO DF Name. Maximum 16 bytes |
| [in] | wNewDFNameLen | [In] Length of new DF Name |
| [in] | pNewISODFName | [In] This means new delegated app ISO DF Name which will replace the existing one. Maximum 16 bytes |
| [out] | pDAMMAC | [Out] Generated 8 bytes DAM MAC for setconfig option 0x06 |
| phStatus_t phalMfdfEVx_CalculateTMV | ( | void * | pDataParams, |
| uint16_t | wOption, | ||
| uint16_t | wKeyNoTMACKey, | ||
| uint16_t | wKeyVerTMACKey, | ||
| uint16_t | wRamKeyNo, | ||
| uint16_t | wRamKeyVer, | ||
| uint8_t * | pDivInput, | ||
| uint8_t | bDivInputLen, | ||
| uint8_t * | pTMC, | ||
| uint8_t * | pUid, | ||
| uint8_t | bUidLen, | ||
| uint8_t * | pTMI, | ||
| uint32_t | dwTMILen, | ||
| uint8_t * | pTMV | ||
| ) |
Computed the Transaction MAC input as performed on the PICC.
While using this command in SAM mode make sure the below points are taken care
KeyNoTMACKey and RamKeyNo should be off Offline_Crypto Keyclass.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | [In] Pointer to this layers parameter structure. |
| [in] | wOption | [In] Diversification option. |
| [in] | wKeyNoTMACKey | [In] Key number to be used from software KeyStore. |
| [in] | wKeyVerTMACKey | [In] Key version to be used from software KeyStore. |
| [in] | wRamKeyNo | [In] Key number of Destination Key where the computed session TMAC key will be stored. To be used for SAM AV3 only. |
| [in] | wRamKeyVer | [In] Key version of Destination Key where the computed session TMAC key will be stored. To be used for SAM AV3 only. |
| [in] | pDivInput | [In] Diversification input to diversify TMACKey. |
| [in] | bDivInputLen | [In] Length of byte available in DivInput buffer. |
| [in] | pTMC | [In] 4 bytes Transaction MAC Counter. It should be 1 time subtracted from the actual value and should be LSB first. |
| [in] | pUid | [In] UID of the card. |
| [in] | bUidLen | [In] Length of UID supplied. |
| [in] | pTMI | [In] Transaction MAC Input. |
| [in] | dwTMILen | [In] Length of bytes available in TMI buffer. |
| [out] | pTMV | [Out] The computed Transaction MAC Value. |
| phStatus_t phalMfdfEVx_DecryptReaderID | ( | void * | pDataParams, |
| uint16_t | wOption, | ||
| uint16_t | wKeyNoTMACKey, | ||
| uint16_t | wKeyVerTMACKey, | ||
| uint16_t | wRamKeyNo, | ||
| uint16_t | wRamKeyVer, | ||
| uint8_t * | pDivInput, | ||
| uint8_t | bDivInputLen, | ||
| uint8_t * | pTMC, | ||
| uint8_t * | pUid, | ||
| uint8_t | bUidLen, | ||
| uint8_t * | pEncTMRI, | ||
| uint8_t * | pTMRIPrev | ||
| ) |
Decrypted the reader ID as performed on the PICC.
While using this command in SAM mode make sure the below points are taken care
KeyNoTMACKey and RamKeyNo should be off Offline_Crypto Keyclass.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | [In] Pointer to this layers parameter structure. |
| [in] | wOption | [In] Diversification option. |
| [in] | wKeyNoTMACKey | [In] Key number to be used from software KeyStore. |
| [in] | wKeyVerTMACKey | [In] Key version to be used from software KeyStore. |
| [in] | wRamKeyNo | [In] Key number of Destination Key where the computed session TMAC key will be stored. To be used for SAM AV3 only. |
| [in] | wRamKeyVer | [In] Key version of Destination Key where the computed session TMAC key will be stored. To be used for SAM AV3 only. |
| [in] | pDivInput | [In] Diversification input to diversify TMACKey. |
| [in] | bDivInputLen | [In] Length of byte available in DivInput buffer. |
| [in] | pTMC | [In] 4 bytes Transaction MAC Counter. It should be 1 time subtracted from the actual value and shold be LSB first. |
| [in] | pUid | [In] UID of the card. |
| [in] | bUidLen | [In] Length of UID supplied. |
| [in] | pEncTMRI | [In] Encrypted Transaction MAC ReaderID of the latest successful transaction. |
| [out] | pTMRIPrev | [Out] Decrypted Reader ID of the last successful transaction. |
| phStatus_t phalMfdfEVx_ComputeMFCLicenseMAC | ( | void * | pDataParams, |
| uint16_t | wOption, | ||
| uint16_t | wMFCLicenseMACKeyNo, | ||
| uint16_t | wMFCLicenseMACKeyVer, | ||
| uint8_t * | pInput, | ||
| uint16_t | wInputLen, | ||
| uint8_t * | pDivInput, | ||
| uint8_t | bDivInputLen, | ||
| uint8_t * | pMFCLicenseMAC | ||
| ) |
Compute the MFCLicenseMAC for phalMfdfEVx_CreateMFCMapping and phalMfdfEVx_RestrictMFCUpdate command.
While using this command in SAM mode make sure the below points are taken care
MFCLicenseMACKeyNo should be off Offline_Crypto Keyclass.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | [In] Pointer to this layers parameter structure. |
| [in] | wOption | [In] Diversification Option. |
| [in] | wMFCLicenseMACKeyNo | [In] Key number in key store for MFCLicenseMAC calculation. |
| [in] | wMFCLicenseMACKeyVer | [In] Key version in key store for MFCLicenseMAC calculation. |
| [in] | pInput | [In] The input for which the MAC should be computed. Input should be as follows. 0x01 || MFCLicense || MFCSectorSecrets |
| [in] | wInputLen | [In] Length of Bytes available in MFCLicenseMACIn buffer. |
| [in] | pDivInput | [In] Diversification input to diversify the Key. |
| [in] | bDivInputLen | [In] Length of Bytes available in DivInput buffer. |
| [out] | pMFCLicenseMAC | [Out] The computed MFCLicense MAC. |
| phStatus_t phalMfdfEVx_CalculateMACSDM | ( | void * | pDataParams, |
| uint8_t | bSdmOption, | ||
| uint16_t | wSDMMacKeyNo, | ||
| uint16_t | wSDMMacKeyVer, | ||
| uint16_t | wRamKeyNo, | ||
| uint16_t | wRamKeyVer, | ||
| uint8_t * | pUid, | ||
| uint8_t | bUidLen, | ||
| uint8_t * | SDMReadCtr, | ||
| uint8_t * | pInData, | ||
| uint16_t | wInDataLen, | ||
| uint8_t * | pRespMac | ||
| ) |
Calculate MAC SDM While using this command in SAM mode make sure the below points are taken care
SDMMacKeyNo and RamKeyNo should be off Offline_Crypto Keyclass.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | [In] Pointer to this layers parameter structure. |
| [in] | bSdmOption | [In] SDM Option to indicate which parameters to be considered. |
| [in] | wSDMMacKeyNo | [In] Key number to be used from software or hardware KeyStore. |
| [in] | wSDMMacKeyVer | [In] Key version to be used from software or hardware KeyStore. |
| [in] | wRamKeyNo | [In] Key number of Destination Key where the computed session TMAC key will be stored. To be used for SAM AV3 only. |
| [in] | wRamKeyVer | [In] Key version of Destination Key where the computed session TMAC key will be stored. To be used for SAM AV3 only. |
| [in] | pUid | [In] UID of the card. |
| [in] | bUidLen | [In] Length of bytes available in pUid buffer. |
| [in] | SDMReadCtr | [In] SDM Read Counter Input. |
| [in] | pInData | [In] Data read out from PICC that is between SDMMacInputoffset until SDMMACOffset. |
| [in] | wInDataLen | [In] Length of bytes available in InData buffer. |
| [out] | pRespMac | [Out] Computed SDM MAC. |
| phStatus_t phalMfdfEVx_DecryptSDMENCFileData | ( | void * | pDataParams, |
| uint8_t | bSdmOption, | ||
| uint16_t | wEncKeyNo, | ||
| uint16_t | wEncKeyVer, | ||
| uint16_t | wRamKeyNo, | ||
| uint16_t | wRamKeyVer, | ||
| uint8_t * | pUid, | ||
| uint8_t | bUidLen, | ||
| uint8_t * | pSDMReadCtr, | ||
| uint8_t * | pEncdata, | ||
| uint16_t | wInDataLen, | ||
| uint8_t * | pPlainData | ||
| ) |
Decrypt SDM enciphered data.
While using this command in SAM mode make sure the below points are taken care
EncKeyNo and RamKeyNo should be off Offline_Crypto Keyclass.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | [In] Pointer to this layers parameter structure. |
| [in] | bSdmOption | [In] SDM Option to indicate which parameters to be considered. |
| [in] | wEncKeyNo | [In] Key number to be used from software or hardware KeyStore. |
| [in] | wEncKeyVer | [In] Key version to be used from software or hardware KeyStore. |
| [in] | wRamKeyNo | [In] Key number of Destination Key where the computed session TMAC key will be stored. To be used for SAM AV3 only. |
| [in] | wRamKeyVer | [In] Key version of Destination Key where the computed session TMAC key will be stored. To be used for SAM AV3 only. |
| [in] | pUid | [In] UID of the card. |
| [in] | bUidLen | [In] Length of bytes available in pUid buffer. |
| [in] | pSDMReadCtr | [In] SDM Read Counter Input. |
| [in] | pEncdata | [In] Encrpted NonASCII SDM Encrypted File data. |
| [in] | wInDataLen | [In] Length of bytes available in EncData buffer. |
| [out] | pPlainData | [Out] The decrypted SDMFile data. |
| phStatus_t phalMfdfEVx_DecryptSDMPICCData | ( | void * | pDataParams, |
| uint16_t | wKeyNo, | ||
| uint16_t | wKeyVer, | ||
| uint8_t * | pEncdata, | ||
| uint16_t | wInDataLen, | ||
| uint8_t * | pPlainData | ||
| ) |
Decrypt SDM PICC Data.
While using this command in SAM mode make sure the below points are taken care
KeyNo should be off Offline_Crypto Keyclass.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | [In] Pointer to this layers parameter structure. |
| [in] | wKeyNo | [In] Key number to be used from software or hardware KeyStore. |
| [in] | wKeyVer | [In] Key version to be used from software or hardware KeyStore. |
| [in] | pEncdata | [In] Encrpted NonASCII SDM PICC data. |
| [in] | wInDataLen | [In] Length of bytes available in EncData buffer. |
| [out] | pPlainData | [Out] The decrypted SDM PICC Data. |
| phStatus_t phalMfdfEVx_SetVCAParams | ( | void * | pDataParams, |
| void * | pAlVCADataParams | ||
| ) |
This is a utility API which sets the VCA structure in DESFire EVx structure params.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | [In] Pointer to this layers parameter structure. |
| [in] | pAlVCADataParams | [In] Pointer to VCA AL parameter structure. |