These Components implement the MIFARE DESFire Light Key Management related commands. More...

Functions | |
| phStatus_t | phalMfdfLight_ChangeKey (void *pDataParams, uint16_t wOption, uint16_t wOldKeyNo, uint16_t wOldKeyVer, uint16_t wNewKeyNo, uint16_t wNewKeyVer, uint8_t bKeyNoCard, uint8_t *pDivInput, uint8_t bDivLen) |
| Changes any key on the PICC. More... | |
| phStatus_t | phalMfdfLight_GetKeyVersion (void *pDataParams, uint8_t bKeyNo, uint8_t bKeySetNo, uint8_t *pKeyVersion, uint8_t *bRxLen) |
| Reads out the current key version of any key stored on the PICC. More... | |
Diversification options to be used with ChangeKey command. | |
| #define | PHAL_MFDFLIGHT_CHGKEY_NO_DIVERSIFICATION 0xFFFFU |
| No diversification. | |
| #define | PHAL_MFDFLIGHT_CHGKEY_DIV_NEW_KEY 0x0002U |
| Bit 1. More... | |
| #define | PHAL_MFDFLIGHT_CHGKEY_DIV_OLD_KEY 0x0004U |
| Bit 2 indicating old key was diversified. | |
| #define | PHAL_MFDFLIGHT_CHGKEY_DIV_NEW_KEY_ONERND 0x0008U |
| Bit 3 indicating new key diversification using one rnd. More... | |
| #define | PHAL_MFDFLIGHT_CHGKEY_DIV_OLD_KEY_ONERND 0x0010U |
| Bit 4 indicating old key diversification using one rnd. More... | |
| #define | PHAL_MFDFLIGHT_CHGKEY_DIV_METHOD_CMAC 0x0020U |
| Bit 5 indicating key diversification method based on CMAC. More... | |
These Components implement the MIFARE DESFire Light Key Management related commands.
| #define PHAL_MFDFLIGHT_CHGKEY_DIV_NEW_KEY 0x0002U |
Bit 1.
Indicating diversification of new key requred.
| #define PHAL_MFDFLIGHT_CHGKEY_DIV_NEW_KEY_ONERND 0x0008U |
Bit 3 indicating new key diversification using one rnd.
Default is two rounds.
| #define PHAL_MFDFLIGHT_CHGKEY_DIV_OLD_KEY_ONERND 0x0010U |
Bit 4 indicating old key diversification using one rnd.
Default is two rounds.
| #define PHAL_MFDFLIGHT_CHGKEY_DIV_METHOD_CMAC 0x0020U |
Bit 5 indicating key diversification method based on CMAC.
Default is Encryption method
| phStatus_t phalMfdfLight_ChangeKey | ( | void * | pDataParams, |
| uint16_t | wOption, | ||
| uint16_t | wOldKeyNo, | ||
| uint16_t | wOldKeyVer, | ||
| uint16_t | wNewKeyNo, | ||
| uint16_t | wNewKeyVer, | ||
| uint8_t | bKeyNoCard, | ||
| uint8_t * | pDivInput, | ||
| uint8_t | bDivLen | ||
| ) |
Changes any key on the PICC.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
| phStatus_t phalMfdfLight_GetKeyVersion | ( | void * | pDataParams, |
| uint8_t | bKeyNo, | ||
| uint8_t | bKeySetNo, | ||
| uint8_t * | pKeyVersion, | ||
| uint8_t * | bRxLen | ||
| ) |
Reads out the current key version of any key stored on the PICC.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bKeyNo | [In] Key number on card. |
| [in] | bKeySetNo | [In] 1 byte Key set number. Optional as it is passed only when bit[6] of bKeyNo is set. |
| [out] | pKeyVersion | [Out] The version of the specified key. |
| [out] | bRxLen | [Out] Length of bytes available in KeyVersion buffer. |