MIFARE DESFire Light PICC (Native) Response Codes | |
| #define | PHAL_MFDFLIGHT_RESP_OPERATION_OK 0x00U |
| MFDFLIGHT Response - Successful operation. | |
| #define | PHAL_MFDFLIGHT_RESP_OK 0x90U |
| MFDFLIGHT Response - Successful operation. | |
| #define | PHAL_MFDFLIGHT_RESP_ERR_CMD_INVALID 0x0BU |
| MFDFLIGHT Invalid Command Error. | |
| #define | PHAL_MFDFLIGHT_RESP_ERR_FORMAT 0x0CU |
| MFDFLIGHT Format Error. | |
| #define | PHAL_MFDFLIGHT_RESP_ERR_OUT_OF_EEPROM_ERROR 0x0EU |
| MFDFLIGHT Response - Insufficient NV-Memory. | |
| #define | PHAL_MFDFLIGHT_RESP_ILLEGAL_COMMAND_CODE 0x1CU |
| MFDFLIGHT command code not supported. | |
| #define | PHAL_MFDFLIGHT_RESP_ERR_INTEGRITY_ERROR 0x1EU |
| MFDFLIGHT CRC or MAC does not match data padding bytes not valid. | |
| #define | PHAL_MFDFLIGHT_RESP_NO_SUCH_KEY 0x40U |
| MFDFLIGHT Invalid key number specified. | |
| #define | PHAL_MFDFLIGHT_RESP_CHAINING 0x71U |
| MFDFLIGHT ISO Chaining Status. | |
| #define | PHAL_MFDFLIGHT_RESP_ERR_LENGTH_ERROR 0x7EU |
| MFDFLIGHT Length of command string invalid. | |
| #define | PHAL_MFDFLIGHT_RESP_PERMISSION_DENIED 0x9DU |
| MFDFLIGHT Current configuration/status does not allow the requested command. | |
| #define | PHAL_MFDFLIGHT_RESP_ERR_PARAMETER_ERROR 0x9EU |
| MFDFLIGHT Value of params invalid. | |
| #define | PHAL_MFDFLIGHT_RESP_APPLICATION_NOT_FOUND 0xA0U |
| MFDFLIGHT Requested AID not found on PICC. | |
| #define | PHAL_MFDFLIGHT_RESP_ERR_APPL_INTEGRITY_ERROR 0xA1U |
| MFDFLIGHT Unrecoverable error within application, appln will be disabled. | |
| #define | PHAL_MFDFLIGHT_RESP_ERR_AUTHENTICATION_ERROR 0xAEU |
| MFDFLIGHT Current authentication status does not allow the requested cmd. | |
| #define | PHAL_MFDFLIGHT_RESP_ERR_AUTHENTICATION_DELAY 0xADU |
| Keep Waiting till Delay is met. | |
| #define | PHAL_MFDFLIGHT_RESP_ADDITIONAL_FRAME 0xAFU |
| MFDFLIGHT Additional data frame is expected to be sent. | |
| #define | PHAL_MFDFLIGHT_RESP_ERR_BOUNDARY_ERROR 0xBEU |
| MFDFLIGHT Attempt to read/write data from/to beyond the files/record's limits. | |
| #define | PHAL_MFDFLIGHT_RESP_ERR_PICC_INTEGRITY 0xC1U |
| MFDFLIGHT Unrecoverable error within PICC. More... | |
| #define | PHAL_MFDFLIGHT_RESP_ERR_COMMAND_ABORTED 0xCAU |
| MFDFLIGHT Previous cmd not fully completed. More... | |
| #define | PHAL_MFDFLIGHT_RESP_ERR_PIC_DISABLED 0xCDU |
| MFDFLIGHT PICC was disabled by an unrecoverable error. | |
| #define | PHAL_MFDFLIGHT_RESP_ERR_COUNT 0xCEU |
| MFDFLIGHT Num. More... | |
| #define | PHAL_MFDFLIGHT_RESP_ERR_DUPLICATE 0xDEU |
| MFDFLIGHT File/Application with same number already exists. | |
| #define | PHAL_MFDFLIGHT_RESP_ERR_EEPROM 0xEEU |
| MFDFLIGHT Could not complete NV-Write operation due to loss of power. | |
| #define | PHAL_MFDFLIGHT_RESP_ERR_FILE_NOT_FOUND 0xF0U |
| MFDFLIGHT Specified file number does not exist. | |
| #define | PHAL_MFDFLIGHT_RESP_ERR_FILE_INTEGRITY 0xF1U |
| MFDFLIGHT Unrecoverable error within file. More... | |
MIFARE DESFire Light PICC (ISO7816) Response Codes | |
| #define | PHAL_MFDFLIGHT_ISO7816_SUCCESS 0x9000U |
| Correct execution. | |
| #define | PHAL_MFDFLIGHT_ISO7816_ERR_WRONG_LENGTH 0x6700U |
| Wrong length. | |
| #define | PHAL_MFDFLIGHT_ISO7816_ERR_WRONG_PARAMS 0x6A86U |
| Wrong parameters P1 and/or P2. | |
| #define | PHAL_MFDFLIGHT_ISO7816_ERR_WRONG_LC 0x6A87U |
| Lc inconsistent with P1/p2. | |
| #define | PHAL_MFDFLIGHT_ISO7816_ERR_WRONG_LE 0x6C00U |
| Wrong Le. | |
| #define | PHAL_MFDFLIGHT_ISO7816_ERR_NO_PRECISE_DIAGNOSTICS 0x6F00U |
| No precise diagnostics. | |
| #define | PHAL_MFDFLIGHT_ISO7816_ERR_EOF_REACHED 0x6282U |
| End of File reached. | |
| #define | PHAL_MFDFLIGHT_ISO7816_ERR_LIMITED_FUNCTIONALITY_INS 0x6283U |
| Limited Functionality. | |
| #define | PHAL_MFDFLIGHT_ISO7816_ERR_FILE_ACCESS 0x6982U |
| File access not allowed. | |
| #define | PHAL_MFDFLIGHT_ISO7816_ERR_FILE_EMPTY 0x6985U |
| File empty or access conditions not satisfied. | |
| #define | PHAL_MFDFLIGHT_ISO7816_ERR_FILE_NOT_FOUND 0x6A82U |
| File not found. | |
| #define | PHAL_MFDFLIGHT_ISO7816_ERR_MEMORY_FAILURE 0x6581U |
| Memory failure (unsuccessful update). | |
| #define | PHAL_MFDFLIGHT_ISO7816_ERR_INCORRECT_PARAMS 0x6B00U |
| Wrong parameter p1 or p2. More... | |
| #define | PHAL_MFDFLIGHT_ISO7816_ERR_WRONG_CLA 0x6E00U |
| Wrong Class byte. | |
| #define | PHAL_MFDFLIGHT_ISO7816_ERR_UNSUPPORTED_INS 0x6D00U |
| Instruction not supported. | |
| #define PHAL_MFDFLIGHT_RESP_ERR_PICC_INTEGRITY 0xC1U |
MFDFLIGHT Unrecoverable error within PICC.
PICC will be disabled.
| #define PHAL_MFDFLIGHT_RESP_ERR_COMMAND_ABORTED 0xCAU |
MFDFLIGHT Previous cmd not fully completed.
Not all frames were requested or provided by the PCD.
| #define PHAL_MFDFLIGHT_RESP_ERR_COUNT 0xCEU |
MFDFLIGHT Num.
of applns limited to 28. No additional applications possible.
| #define PHAL_MFDFLIGHT_RESP_ERR_FILE_INTEGRITY 0xF1U |
MFDFLIGHT Unrecoverable error within file.
File will be disabled.
| #define PHAL_MFDFLIGHT_ISO7816_ERR_INCORRECT_PARAMS 0x6B00U |
Wrong parameter p1 or p2.
READ RECORDS.