Data Structures | |
| struct | phalMfdfLight_SamAV3_NonX_DataParams_t |
| MIFARE DESfire Light SAM AV3 NonX parameter structure More... | |
Macros | |
| #define | PHAL_MFDFLIGHT_SAMAV3_NONX_ID 0x02U |
| ID for SamAV3 Non X MF DesFire LIGHT layer. | |
Functions | |
| phStatus_t | phalMfdfLight_SamAV3_NonX_Init (phalMfdfLight_SamAV3_NonX_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, phhalHw_SamAV3_DataParams_t *pHalSamDataParams, void *pPalMifareDataParams, phTMIUtils_t *pTMIDataParams) |
| Initializes the DESFire Light Sam AV3 component in Non X mode (S mode). More... | |
| phStatus_t phalMfdfLight_SamAV3_NonX_Init | ( | phalMfdfLight_SamAV3_NonX_DataParams_t * | pDataParams, |
| uint16_t | wSizeOfDataParams, | ||
| phhalHw_SamAV3_DataParams_t * | pHalSamDataParams, | ||
| void * | pPalMifareDataParams, | ||
| phTMIUtils_t * | pTMIDataParams | ||
| ) |
Initializes the DESFire Light Sam AV3 component in Non X mode (S mode).
| PH_ERR_SUCCESS | Operation successful. |
| PH_ERR_INVALID_DATA_PARAMS | for Invaid Dataparams |
| PH_ERR_INVALID_PARAMETER | for invalid parameter values. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | wSizeOfDataParams | [In] Specifies the size of the data parameter structure |
| [in] | pHalSamDataParams | [In] Pointer to the HAL parameter structure of the SAM. |
| [in] | pPalMifareDataParams | [In] Pointer to Pal Mifare parameter structure. |
| [in] | pTMIDataParams | [In] Pointer to the parameter structure for collecting TMI. |