NXP Reader Library  v17.1.0.2535
Commands_TransactionManagement

These Components implement the MIFARE DESFire Light Transaction Management related commands. More...

Collaboration diagram for Commands_TransactionManagement:

Functions

phStatus_t phalMfdfLight_CommitTransaction (void *pDataParams, uint8_t bOption, uint8_t *pTMC, uint8_t *pTMV)
 Validates all previous write access' on Backup Data files, value files and record files within one application. More...
 
phStatus_t phalMfdfLight_AbortTransaction (void *pDataParams)
 Invalidates all previous write access' on Backup Data files, value files and record files within one application. More...
 
phStatus_t phalMfdfLight_CommitReaderID (void *pDataParams, uint8_t *pTMRI, uint8_t *pEncTMRI)
 Secures the transaction by commiting the application to ReaderID specified. More...
 

Options for CommitTransaction command.

#define PHAL_MFDFLIGHT_COMMIT_TXN_NO_TMC_TMV_RETURNED   0x00
 Option byte is not exchanged to the PICC.
 
#define PHAL_MFDFLIGHT_COMMIT_TXN_TMC_TMV_RETURNED   0x01
 Option byte exchanged to PICC and represent return of TMC and TMV.
 
#define PHAL_MFDFLIGHT_COMMIT_TXN_INCLUDE_OPTION   0x80
 Option byte exchanged to PICC. More...
 

Detailed Description

These Components implement the MIFARE DESFire Light Transaction Management related commands.

Macro Definition Documentation

◆ PHAL_MFDFLIGHT_COMMIT_TXN_INCLUDE_OPTION

#define PHAL_MFDFLIGHT_COMMIT_TXN_INCLUDE_OPTION   0x80

Option byte exchanged to PICC.

This is to support the exchange of Option byte to PICC.

Function Documentation

◆ phalMfdfLight_CommitTransaction()

phStatus_t phalMfdfLight_CommitTransaction ( void *  pDataParams,
uint8_t  bOption,
uint8_t pTMC,
uint8_t pTMV 
)

Validates all previous write access' on Backup Data files, value files and record files within one application.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]bOption[In] One of the below options.
[out]pTMC[Out] The increased value as stored in FileType.TransactionMAC.
If Standard AES: 4 byte Transaction MAC counter value.
If LRP : 2 byte of Actual TMC followed by 2 bytes of Session TMC
[out]pTMV[Out] 8 bytes Transaction MAC value.

◆ phalMfdfLight_AbortTransaction()

phStatus_t phalMfdfLight_AbortTransaction ( void *  pDataParams)

Invalidates all previous write access' on Backup Data files, value files and record files within one application.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.

◆ phalMfdfLight_CommitReaderID()

phStatus_t phalMfdfLight_CommitReaderID ( void *  pDataParams,
uint8_t pTMRI,
uint8_t pEncTMRI 
)

Secures the transaction by commiting the application to ReaderID specified.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]pTMRI[In] 16 bytes of Transaction MAC reader ID.
[out]pEncTMRI[Out] 16 bytes of Encrypted Transaction MAC ReaderID of the latest successful transaction.