These Components implement the custom error codes mapped to PICC return codes. These are the values that will be returned to the user from the interface in case of error. More...

Custom Error Codes mapping for PICC erro codes | |
| #define | PHAL_MFDF_NO_CHANGES (PH_ERR_CUSTOM_BEGIN + 0) |
| DESFire Response - No changes done to backup files. | |
| #define | PHAL_MFDF_ERR_OUT_OF_EEPROM_ERROR (PH_ERR_CUSTOM_BEGIN + 1) |
| DESFire Response - Insufficient NV-Memory. | |
| #define | PHAL_MFDF_ERR_NO_SUCH_KEY (PH_ERR_CUSTOM_BEGIN + 2) |
| DESFire Invalid key number specified. | |
| #define | PHAL_MFDF_ERR_PERMISSION_DENIED (PH_ERR_CUSTOM_BEGIN + 3) |
| DESFire Current configuration/status does not allow the requested command. | |
| #define | PHAL_MFDF_ERR_APPLICATION_NOT_FOUND (PH_ERR_CUSTOM_BEGIN + 4) |
| DESFire Requested AID not found on PICC. | |
| #define | PHAL_MFDF_ERR_BOUNDARY_ERROR (PH_ERR_CUSTOM_BEGIN + 5) |
| DESFire Attempt to read/write data from/to beyond the files/record's limits. | |
| #define | PHAL_MFDF_ERR_COMMAND_ABORTED (PH_ERR_CUSTOM_BEGIN + 6) |
| DESFire Previous cmd not fully completed. More... | |
| #define | PHAL_MFDF_ERR_COUNT (PH_ERR_CUSTOM_BEGIN + 7) |
| DESFire Num. More... | |
| #define | PHAL_MFDF_ERR_DUPLICATE (PH_ERR_CUSTOM_BEGIN + 8) |
| DESFire File/Application with same number already exists. | |
| #define | PHAL_MFDF_ERR_FILE_NOT_FOUND (PH_ERR_CUSTOM_BEGIN + 9) |
| DESFire Specified file number does not exist. | |
| #define | PHAL_MFDF_ERR_PICC_CRYPTO (PH_ERR_CUSTOM_BEGIN + 10) |
| DESFire Crypto error returned by PICC. | |
| #define | PHAL_MFDF_ERR_PARAMETER_ERROR (PH_ERR_CUSTOM_BEGIN + 11) |
| DESFire Parameter value error returned by PICC. | |
| #define | PHAL_MFDF_ERR_DF_GEN_ERROR (PH_ERR_CUSTOM_BEGIN + 12) |
| DESFire DesFire Generic error. More... | |
| #define | PHAL_MFDF_ERR_DF_7816_GEN_ERROR (PH_ERR_CUSTOM_BEGIN + 13) |
| DESFire ISO 7816 Generic error. More... | |
These Components implement the custom error codes mapped to PICC return codes. These are the values that will be returned to the user from the interface in case of error.
| #define PHAL_MFDF_ERR_COMMAND_ABORTED (PH_ERR_CUSTOM_BEGIN + 6) |
DESFire Previous cmd not fully completed.
Not all frames were requested or provided by the PCD.
| #define PHAL_MFDF_ERR_COUNT (PH_ERR_CUSTOM_BEGIN + 7) |
DESFire Num.
of applns limited to 28. No additional applications possible.
| #define PHAL_MFDF_ERR_DF_GEN_ERROR (PH_ERR_CUSTOM_BEGIN + 12) |
DESFire DesFire Generic error.
Check additional Info.
| #define PHAL_MFDF_ERR_DF_7816_GEN_ERROR (PH_ERR_CUSTOM_BEGIN + 13) |
DESFire ISO 7816 Generic error.
Check Additional Info.