These Components implement the actual PICC error codes. These are the values that will not be returned to the user from the interface in case of error. More...

MIFARE Desfire PICC Response Codes | |
| #define | PHAL_MFDF_RESP_OPERATION_OK 0x00U |
| MF DF Response - Successful operation. | |
| #define | PHAL_MFDF_RESP_NO_CHANGES 0x0CU |
| MF DF Response - No changes done to backup files. | |
| #define | PHAL_MFDF_RESP_ERR_OUT_OF_EEPROM_ERROR 0x0EU |
| MF DF Response - Insufficient NV-Memory. | |
| #define | PHAL_MFDF_RESP_ILLEGAL_COMMAND_CODE 0x1CU |
| MF DF command code not supported. | |
| #define | PHAL_MFDF_RESP_ERR_INTEGRITY_ERROR 0x1EU |
| MF DF CRC or MAC does not match data padding bytes not valid. | |
| #define | PHAL_MFDF_RESP_NO_SUCH_KEY 0x40U |
| MF DF Invalid key number specified. | |
| #define | PHAL_MFDF_RESP_ERR_LENGTH_ERROR 0x7EU |
| MF DF Length of command string invalid. | |
| #define | PHAL_MFDF_RESP_PERMISSION_DENIED 0x9DU |
| MF DF Current configuration/status does not allow the requested command. | |
| #define | PHAL_MFDF_RESP_ERR_PARAMETER_ERROR 0x9EU |
| MF DF Value of params invalid. | |
| #define | PHAL_MFDF_RESP_APPLICATION_NOT_FOUND 0xA0U |
| MF DF Requested AID not found on PICC. | |
| #define | PHAL_MFDF_RESP_ERR_APPL_INTEGRITY_ERROR 0xA1U |
| MF DF Unrecoverable error within application, appln will be disabled. | |
| #define | PHAL_MFDF_RESP_ERR_AUTHENTICATION_ERROR 0xAEU |
| MF DF Current authentication status does not allow the requested cmd. | |
| #define | PHAL_MFDF_RESP_ADDITIONAL_FRAME 0xAFU |
| MF DF Additional data frame is expected to be sent. | |
| #define | PHAL_MFDF_RESP_ERR_BOUNDARY_ERROR 0xBEU |
| MF DF Attempt to read/write data from/to beyond the files/record's limits. | |
| #define | PHAL_MFDF_RESP_ERR_PICC_INTEGRITY 0xC1U |
| MF DF Unrecoverable error within PICC. More... | |
| #define | PHAL_MFDF_RESP_ERR_COMMAND_ABORTED 0xCAU |
| MF DF Previous cmd not fully completed. More... | |
| #define | PHAL_MFDF_RESP_ERR_PIC_DISABLED 0xCDU |
| MF DF PICC was disabled by an unrecoverable error. | |
| #define | PHAL_MFDF_RESP_ERR_COUNT 0xCEU |
| MF DF Num. More... | |
| #define | PHAL_MFDF_RESP_ERR_DUPLICATE 0xDEU |
| MF DF File/Application with same number already exists. | |
| #define | PHAL_MFDF_RESP_ERR_EEPROM 0xEEU |
| MF DF Could not complete NV-Write operation due to loss of power. | |
| #define | PHAL_MFDF_RESP_ERR_FILE_NOT_FOUND 0xF0U |
| MF DF Specified file number does not exist. | |
| #define | PHAL_MFDF_RESP_ERR_FILE_INTEGRITY 0xF1U |
| MF DF Unrecoverable error within file. More... | |
MIFARE Desfire PICC ISO7816 Response Codes | |
| #define | PHAL_MFDF_ISO7816_SUCCESS 0x9000U |
| Correct execution. | |
| #define | PHAL_MFDF_ISO7816_ERR_WRONG_LENGTH 0x6700U |
| Wrong length. | |
| #define | PHAL_MFDF_ISO7816_ERR_INVALID_APPLN 0x6A82U |
| Application / file not found. | |
| #define | PHAL_MFDF_ISO7816_ERR_WRONG_PARAMS 0x6A86U |
| Wrong parameters P1 and/or P2. | |
| #define | PHAL_MFDF_ISO7816_ERR_WRONG_LC 0x6A87U |
| Lc inconsistent with P1/p2. | |
| #define | PHAL_MFDF_ISO7816_ERR_WRONG_LE 0x6C00U |
| Wrong Le. | |
| #define | PHAL_MFDF_ISO7816_ERR_NO_PRECISE_DIAGNOSTICS 0x6F00U |
| No precise diagnostics. | |
| #define | PHAL_MFDF_ISO7816_ERR_EOF_REACHED 0x6282U |
| End of File reached. | |
| #define | PHAL_MFDF_ISO7816_ERR_FILE_ACCESS 0x6982U |
| File access not allowed. | |
| #define | PHAL_MFDF_ISO7816_ERR_FILE_EMPTY 0x6985U |
| File empty or access conditions not satisfied. | |
| #define | PHAL_MFDF_ISO7816_ERR_FILE_NOT_FOUND 0x6A82U |
| File not found. | |
| #define | PHAL_MFDF_ISO7816_ERR_MEMORY_FAILURE 0x6581U |
| Memory failure (unsuccessful update). | |
| #define | PHAL_MFDF_ISO7816_ERR_INCORRECT_PARAMS 0x6B00U |
| Wrong parameter p1 or p2. More... | |
| #define | PHAL_MFDF_ISO7816_ERR_WRONG_CLA 0x6E00U |
| Wrong Class byte. | |
| #define | PHAL_MFDF_ISO7816_ERR_UNSUPPORTED_INS 0x6D00U |
| Instruction not supported. | |
These Components implement the actual PICC error codes. These are the values that will not be returned to the user from the interface in case of error.
| #define PHAL_MFDF_RESP_ERR_PICC_INTEGRITY 0xC1U |
MF DF Unrecoverable error within PICC.
PICC will be disabled.
| #define PHAL_MFDF_RESP_ERR_COMMAND_ABORTED 0xCAU |
MF DF Previous cmd not fully completed.
Not all frames were requested or provided by the PCD.
| #define PHAL_MFDF_RESP_ERR_COUNT 0xCEU |
MF DF Num.
of applns limited to 28. No additional applications possible.
| #define PHAL_MFDF_RESP_ERR_FILE_INTEGRITY 0xF1U |
MF DF Unrecoverable error within file.
File will be disabled.
| #define PHAL_MFDF_ISO7816_ERR_INCORRECT_PARAMS 0x6B00U |
Wrong parameter p1 or p2.
READ RECORDS.