NXP Reader Library  v17.1.0.2535
Component : Sam_NonX
Collaboration diagram for Component : Sam_NonX:

Data Structures

struct  phalMfdf_SamAV2_DataParams_t
 MIFARE DESfire SAM AV2 NonX parameter structure
More...
 
struct  phalMfdf_SamAV3_NonX_DataParams_t
 MIFARE DESfire SAM AV3 NonX parameter structure
More...
 

Macros

#define PHAL_MFDF_SAMAV2_ID   0x02U
 ID for SamAV2 MF DesFire layer.
 
#define PHAL_MFDF_SAMAV3_NONX_ID   0x04U
 ID for SamAV3 MF DesFire layer.
 

Functions

phStatus_t phalMfdf_SamAV2_Init (phalMfdf_SamAV2_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, phhalHw_SamAV2_DataParams_t *pHalSamDataParams, void *pHalDataParams, void *pPalMifareDataParams)
 Initialise SAM AV2 NonX layer. More...
 
phStatus_t phalMfdf_SamAV3_NonX_Init (phalMfdf_SamAV3_NonX_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, phhalHw_SamAV3_DataParams_t *pHalSamDataParams, void *pPalMifareDataParams)
 Initialise SAM AV3 NonX layer. More...
 

Detailed Description

Function Documentation

◆ phalMfdf_SamAV2_Init()

phStatus_t phalMfdf_SamAV2_Init ( phalMfdf_SamAV2_DataParams_t pDataParams,
uint16_t  wSizeOfDataParams,
phhalHw_SamAV2_DataParams_t pHalSamDataParams,
void *  pHalDataParams,
void *  pPalMifareDataParams 
)

Initialise SAM AV2 NonX layer.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]wSizeOfDataParams[In] Specifies the size of the data parameter structure
[in]pHalSamDataParams[In] Pointer to the HAL parameter structure of the SAM.
[in]pHalDataParams[In] Pointer to HAL param structure of contactless reader.
[in]pPalMifareDataParams[In] Pointer to the parameter structure of the underlying palMIFARE layer.

◆ phalMfdf_SamAV3_NonX_Init()

phStatus_t phalMfdf_SamAV3_NonX_Init ( phalMfdf_SamAV3_NonX_DataParams_t pDataParams,
uint16_t  wSizeOfDataParams,
phhalHw_SamAV3_DataParams_t pHalSamDataParams,
void *  pPalMifareDataParams 
)

Initialise SAM AV3 NonX layer.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]wSizeOfDataParams[In] Specifies the size of the data parameter structure
[in]pHalSamDataParams[In] Pointer to the HAL parameter structure of the SAM.
[in]pPalMifareDataParams[In] Pointer to the parameter structure of the underlying palMIFARE layer.