These Components implement the MIFARE Plus (EVx, EV2, future versions) commands. More...

Modules | |
| Component : Software | |
| Component : Sam_NonX | |
| Component : Sam_X | |
| ErrorCodes | |
| These component implement the MIFARE Plus (EVx, EV2, future versions) Error codes. | |
| Common Definitions | |
| These are common definitions for most of the Plus commands. | |
| Commands_Personalization | |
| These Components implement the MIFARE Plus EVx personalization commands. | |
| Commands_Authenticate | |
| These Components implement the MIFARE Plus EVx authentication commands. | |
| Commands_DataOperations | |
| These Components implement the MIFARE Plus EVx data operation commands. | |
| Commands_ValueOperations | |
| These Components implement the MIFARE Plus EVx value operation commands. | |
| Commands_Special | |
| These Components implement the MIFARE Plus EVx additional feature commands. | |
| Utilities | |
| These Components implement the utility interfaces required for MIFARE Plus EVx application layer. These are not commands. | |
These Components implement the MIFARE Plus (EVx, EV2, future versions) commands.