NXP Reader Library  v17.1.0.2535

These Components implement the custom error codes mapped to PICC return codes. These are the values that will be returned to the user from the interface in case of error. More...

Collaboration diagram for Custom ErrorCodes:

Custom Error Codes mapping for PICC erro codes.

#define PHAL_MFPEVX_ERR_AUTH   (PH_ERR_CUSTOM_BEGIN + 0U)
 MFP EVx Authentication Error. More...
 
#define PHAL_MFPEVX_ERR_CMD_OVERFLOW   (PH_ERR_CUSTOM_BEGIN + 1U)
 MFP EVx Command Overflow Error. More...
 
#define PHAL_MFPEVX_ERR_MAC_PCD   (PH_ERR_CUSTOM_BEGIN + 2U)
 MFP EVx MAC Error. More...
 
#define PHAL_MFPEVX_ERR_BNR   (PH_ERR_CUSTOM_BEGIN + 3U)
 MFP EVx Blocknumber Error. More...
 
#define PHAL_MFPEVX_ERR_EXT   (PH_ERR_CUSTOM_BEGIN + 4U)
 MFP EVx Extension Error. More...
 
#define PHAL_MFPEVX_ERR_CMD_INVALID   (PH_ERR_CUSTOM_BEGIN + 5U)
 MFP EVx Invalid Command Error. More...
 
#define PHAL_MFPEVX_ERR_FORMAT   (PH_ERR_CUSTOM_BEGIN + 6U)
 MFP EVx Authentication Error. More...
 
#define PHAL_MFPEVX_ERR_GEN_FAILURE   (PH_ERR_CUSTOM_BEGIN + 7U)
 MFP EVx Generic Error. More...
 
#define PHAL_MFPEVX_ERR_TM   (PH_ERR_CUSTOM_BEGIN + 8U)
 MFP EVx Transaction MAC related Error. More...
 
#define PHAL_MFPEVX_ERR_NOT_SUP   (PH_ERR_CUSTOM_BEGIN + 9U)
 MFP EVx Not Supported Error. More...
 
#define PHAL_MFPEVX_ISO7816_ERR_WRONG_LENGTH   (PH_ERR_CUSTOM_BEGIN + 10U)
 MFP EVx 7816 wrong length error. More...
 
#define PHAL_MFPEVX_ISO7816_ERR_WRONG_PARAMS   (PH_ERR_CUSTOM_BEGIN + 11U)
 MFP EVx 7816 wrong params error. More...
 
#define PHAL_MFPEVX_ISO7816_ERR_WRONG_LC   (PH_ERR_CUSTOM_BEGIN + 12U)
 MFP EVx 7816 wrong Lc error. More...
 
#define PHAL_MFPEVX_ISO7816_ERR_WRONG_LE   (PH_ERR_CUSTOM_BEGIN + 13U)
 MFP EVx 7816 wrong LE error. More...
 
#define PHAL_MFPEVX_ISO7816_ERR_WRONG_CLA   (PH_ERR_CUSTOM_BEGIN + 14U)
 MFP EVx 7816 wrong CLA error. More...
 

Detailed Description

These Components implement the custom error codes mapped to PICC return codes. These are the values that will be returned to the user from the interface in case of error.

Macro Definition Documentation

◆ PHAL_MFPEVX_ERR_AUTH

#define PHAL_MFPEVX_ERR_AUTH   (PH_ERR_CUSTOM_BEGIN + 0U)

MFP EVx Authentication Error.

This error represents PICC's PHAL_MFPEVX_RESP_ERR_AUTH error.

◆ PHAL_MFPEVX_ERR_CMD_OVERFLOW

#define PHAL_MFPEVX_ERR_CMD_OVERFLOW   (PH_ERR_CUSTOM_BEGIN + 1U)

MFP EVx Command Overflow Error.

This error represents PICC's PHAL_MFPEVX_RESP_ERR_CMD_OVERFLOW error.

◆ PHAL_MFPEVX_ERR_MAC_PCD

#define PHAL_MFPEVX_ERR_MAC_PCD   (PH_ERR_CUSTOM_BEGIN + 2U)

MFP EVx MAC Error.

This error represents PICC's PHAL_MFPEVX_RESP_ERR_MAC_PCD error.

◆ PHAL_MFPEVX_ERR_BNR

#define PHAL_MFPEVX_ERR_BNR   (PH_ERR_CUSTOM_BEGIN + 3U)

MFP EVx Blocknumber Error.

This error represents PICC's PHAL_MFPEVX_RESP_ERR_BNR error.

◆ PHAL_MFPEVX_ERR_EXT

#define PHAL_MFPEVX_ERR_EXT   (PH_ERR_CUSTOM_BEGIN + 4U)

MFP EVx Extension Error.

This error represents PICC's PHAL_MFPEVX_RESP_ERR_EXT error.

◆ PHAL_MFPEVX_ERR_CMD_INVALID

#define PHAL_MFPEVX_ERR_CMD_INVALID   (PH_ERR_CUSTOM_BEGIN + 5U)

MFP EVx Invalid Command Error.

This error represents PICC's PHAL_MFPEVX_RESP_ERR_CMD_INVALID error.

◆ PHAL_MFPEVX_ERR_FORMAT

#define PHAL_MFPEVX_ERR_FORMAT   (PH_ERR_CUSTOM_BEGIN + 6U)

MFP EVx Authentication Error.

This error represents PICC's PHAL_MFPEVX_RESP_ERR_FORMAT error.

◆ PHAL_MFPEVX_ERR_GEN_FAILURE

#define PHAL_MFPEVX_ERR_GEN_FAILURE   (PH_ERR_CUSTOM_BEGIN + 7U)

MFP EVx Generic Error.

This error represents PICC's PHAL_MFPEVX_RESP_ERR_GEN_FAILURE error.

◆ PHAL_MFPEVX_ERR_TM

#define PHAL_MFPEVX_ERR_TM   (PH_ERR_CUSTOM_BEGIN + 8U)

MFP EVx Transaction MAC related Error.

This error represents PICC's PHAL_MFPEVX_RESP_ERR_TM error.

◆ PHAL_MFPEVX_ERR_NOT_SUP

#define PHAL_MFPEVX_ERR_NOT_SUP   (PH_ERR_CUSTOM_BEGIN + 9U)

MFP EVx Not Supported Error.

This error represents PICC's PHAL_MFPEVX_RESP_ERR_NOT_SUP error.

◆ PHAL_MFPEVX_ISO7816_ERR_WRONG_LENGTH

#define PHAL_MFPEVX_ISO7816_ERR_WRONG_LENGTH   (PH_ERR_CUSTOM_BEGIN + 10U)

MFP EVx 7816 wrong length error.

This error represents PICC's PHAL_MFPEVX_ISO7816_RESP_ERR_WRONG_LENGTH error.

◆ PHAL_MFPEVX_ISO7816_ERR_WRONG_PARAMS

#define PHAL_MFPEVX_ISO7816_ERR_WRONG_PARAMS   (PH_ERR_CUSTOM_BEGIN + 11U)

MFP EVx 7816 wrong params error.

This error represents PICC's PHAL_MFPEVX_ISO7816_RESP_ERR_WRONG_PARAMS error.

◆ PHAL_MFPEVX_ISO7816_ERR_WRONG_LC

#define PHAL_MFPEVX_ISO7816_ERR_WRONG_LC   (PH_ERR_CUSTOM_BEGIN + 12U)

MFP EVx 7816 wrong Lc error.

This error represents PICC's PHAL_MFPEVX_ISO7816_RESP_ERR_WRONG_LC error.

◆ PHAL_MFPEVX_ISO7816_ERR_WRONG_LE

#define PHAL_MFPEVX_ISO7816_ERR_WRONG_LE   (PH_ERR_CUSTOM_BEGIN + 13U)

MFP EVx 7816 wrong LE error.

This error represents PICC's PHAL_MFPEVX_ISO7816_RESP_ERR_WRONG_LE error.

◆ PHAL_MFPEVX_ISO7816_ERR_WRONG_CLA

#define PHAL_MFPEVX_ISO7816_ERR_WRONG_CLA   (PH_ERR_CUSTOM_BEGIN + 14U)

MFP EVx 7816 wrong CLA error.

This error represents PICC's PHAL_MFPEVX_ISO7816_RESP_ERR_WRONG_CLA error.