These Components implement the MIFARE Plus EVx data operation commands.
More...
|
| phStatus_t | phalMfpEVx_Write (void *pDataParams, uint8_t bEncrypted, uint8_t bWriteMaced, uint16_t wBlockNr, uint8_t bNumBlocks, uint8_t *pBlocks, uint8_t *pTMC, uint8_t *pTMV) |
| | Performs a Write / Write MACed command. More...
|
| |
| phStatus_t | phalMfpEVx_Read (void *pDataParams, uint8_t bEncrypted, uint8_t bReadMaced, uint8_t bMacOnCmd, uint16_t wBlockNr, uint8_t bNumBlocks, uint8_t *pBlocks) |
| | Performs a Read / Read MACed command. More...
|
| |
These Components implement the MIFARE Plus EVx data operation commands.
◆ phalMfpEVx_Write()
Performs a Write / Write MACed command.
This command writes a 16 byte data to the PICC. The parameter Encrypted, WriteMaced are valid only for MFP authenticated state and not for MFC authenticate state.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bEncrypted | [In] Type of communication to be used. Based on this flag the command code will be updated.
|
| [in] | bWriteMaced | [In] Indicate whether the response should be maced. Based on this flag the command code will be updated.
|
| [in] | wBlockNr | [In] PICC block number to which the data should be written. |
| [in] | bNumBlocks | [In] Number of blocks to write.
15 block for Native communication if configured as Software component.
13 blocks if configured as Sam X or Sam NonX component. |
| [in] | pBlocks | [In] The data to be written. This buffer should have data equal to NumBlocks * 16, where 16 is one block size. |
| [out] | pTMC | [Out] Only available is the block is a TMProtected block. The buffer will have 4 bytes of Transaction MAC counter information. |
| [out] | pTMV | [Out] Only available is the block is a TMProtected block. The buffer will have 8 bytes of Transaction MAC value. |
◆ phalMfpEVx_Read()
Performs a Read / Read MACed command.
The parameter Encrypted, ReadMaced and MacOnCmd are valid only for MFP authenticated state and not for MFC authenticate state.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bEncrypted | [In] Type of communication to be used. Based on this flag the command code will be updated.
|
| [in] | bReadMaced | [In] Indicate whether the response should be maced. Based on this flag the command code will be updated.
|
| [in] | bMacOnCmd | [In] Indicate whether the command should be maced. Based on this flag the command code will be updated.
|
| [in] | wBlockNr | [In] PICC block number from which the data should be read. |
| [in] | bNumBlocks | [In] Number of blocks to be read.
15 block for Native communication if configured as Software component.
13 blocks if configured as Sam X or Sam NonX component. |
| [out] | pBlocks | [Out] The data to be read. This buffer should have data equal to ((NumBlocks * 16) + 8), where 16 is one block size and 8 bytes is for storing the MAC received form PICC. The last 8 bytes will be cleared once returned to the application. |