Data Structures | |
| struct | phalMfp_Sw_DataParams_t |
| MIFARE Plus Software parameter structure. More... | |
Macros | |
| #define | PHAL_MFP_SW_ID 0x01 |
| ID for Software MIFARE Plus layer. | |
Functions | |
| phStatus_t | phalMfp_Sw_Init (phalMfp_Sw_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, void *pPalMifareDataParams, void *pKeyStoreDataParams, void *pCryptoDataParamsEnc, void *pCryptoDataParamsMac, void *pCryptoRngDataParams, void *pCryptoDiversifyDataParams) |
| Initialise this layer. More... | |
| phStatus_t phalMfp_Sw_Init | ( | phalMfp_Sw_DataParams_t * | pDataParams, |
| uint16_t | wSizeOfDataParams, | ||
| void * | pPalMifareDataParams, | ||
| void * | pKeyStoreDataParams, | ||
| void * | pCryptoDataParamsEnc, | ||
| void * | pCryptoDataParamsMac, | ||
| void * | pCryptoRngDataParams, | ||
| void * | pCryptoDiversifyDataParams | ||
| ) |
Initialise this layer.
| PH_ERR_SUCCESS | Operation successful. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | wSizeOfDataParams | [In] Specifies the size of the data parameter structure. |
| [in] | pPalMifareDataParams | [In] Pointer to a palMifare component context. |
| [in] | pKeyStoreDataParams | [In] Pointer to a KeyStore component context. |
| [in] | pCryptoDataParamsEnc | [In] Pointer to a Crypto component context for encryption. |
| [in] | pCryptoDataParamsMac | [In] Pointer to a Crypto component context for Macing. |
| [in] | pCryptoRngDataParams | [In] Pointer to a CryptoRng component context. |
| [in] | pCryptoDiversifyDataParams | [In] Pointer to the parameter structure of the CryptoDiversify layer (can be NULL). |