This is only a wrapper layer to abstract the different NTAG X DNA implementations. With this wrapper it is possible to support more than one NTAG X DNA implementation in parallel, by adapting this wrapper. More...

Modules | |
| Component : Software | |
| Software implementation of the NTAG X DNA commands. Here the NTAG X DNA commands are framed and exchanged to tag. | |
| ErrorCodes | |
| Error Codes received from tag and the equivalent Reader Library error codes. | |
| Defines | |
| Commands_SecureMessaging | |
| Describes about the NTAG X DNA Secure Messaging related commands. | |
| Commands_MemoryConfiguration | |
| Describes about the NTAG X DNA Memory and Configuration Management commands. | |
| Commands_SymmetricKeyManagement | |
| Describes about the NTAG X DNA Symmetric Key Management commands. | |
| Commands_ASymmetricKeyManagement | |
| Describes about the NTAG X DNA ASymmetric Key Management commands. | |
| Commands_CertificateKeyManagement | |
| Describes about the NTAG X DNA Certificate Management commands. | |
| Commands_FileManagement | |
| Describes about the NTAG X DNA File Management commands. | |
| Commands_DataManagement | |
| Describes about the NTAG X DNA Data Management commands. | |
| Commands_CryptoAPI | |
| Describes about the NTAG X DNA Crypto API commands. | |
| Commands_GPIOManagement | |
| Describes about the NTAG X DNA GPIO management commands. | |
| Commands_ISO7816 | |
| Describes about the NTAG X DNA ISO/IEC 7816-4 Standard commands. | |
| Commands_Utility | |
| Describes about the NTAG X DNA Utility functions. These are not part of actual NTAG X DNA data sheet rather its for internal purpose. | |
This is only a wrapper layer to abstract the different NTAG X DNA implementations. With this wrapper it is possible to support more than one NTAG X DNA implementation in parallel, by adapting this wrapper.