Describes about the NTAG X DNA Symmetric Key Management commands.
More...
|
| | Defines |
| | Macro Definitions for Symmetric Key Management commands.
|
| |
|
| phStatus_t | phalNtagXDna_ChangeKey (void *pDataParams, uint16_t wOption, uint16_t wCurrKeyNo, uint16_t wCurrKeyVer, uint16_t wNewKeyNo, uint16_t wNewKeyVer, uint8_t bKeyNoCard, uint8_t *pKeyPolicy, uint8_t *pDivInput, uint8_t bDivLen) |
| | Depending on the currently selected AID, this command update a key of the tag or of an application AKS (Active Key Set). More...
|
| |
| phStatus_t | phalNtagXDna_GetKeySettings (void *pDataParams, uint8_t bOption, uint8_t **ppResponse, uint16_t *pRspLen) |
| | Gets Application Key Setting for the application. More...
|
| |
| phStatus_t | phalNtagXDna_GetKeyVersion (void *pDataParams, uint8_t bKeyNo, uint8_t **ppResponse, uint16_t *pRspLen) |
| | Reads out the current key version of any key stored on the tag. More...
|
| |
Describes about the NTAG X DNA Symmetric Key Management commands.
◆ phalNtagXDna_ChangeKey()
Depending on the currently selected AID, this command update a key of the tag or of an application AKS (Active Key Set).
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | wOption | [In] Option to be used for diversifying the Current and New key.
|
| [in] | wCurrKeyNo | [In] Current key number in KeyStore of software. |
| [in] | wCurrKeyVer | [In] Current key version in KeyStore of software. |
| [in] | wNewKeyNo | [In] New key number in KeyStore of software. |
| [in] | wNewKeyVer | [In] New key version in KeyStore of software. |
| [in] | bKeyNoCard | [In] Key number of the key to be changed. To be ORed with
- Bit[7 - 6]:
- With the type of the key if targeting AppMasterKey or CryptoRequestKey,
- 10 : KeyType.AES128
- 11 : KeyType.AES256
- RFU otherwise
- Bit[5 - 0]: Application Master or CryptoRequest Key.
- 0x00 - 0x04: Application Keys
- 0x10 - 0x17: CryptoRequest Keys
|
| [in] | pKeyPolicy | [In] Defines the allowed crypto operations with the targeted key. Optional present if targeting CryptoRequest Key.
|
| [in] | pDivInput | [In] Diversification input to be used for diversifying the key. Can be NULL. |
| [in] | bDivLen | [In] Length of bytes available in pDivInput buffer. |
◆ phalNtagXDna_GetKeySettings()
Gets Application Key Setting for the application.
In addition it returns the number of keys which are configured for the selected application and if applicable the AppKeySetSettings.
Note: The Option information will not be exchanged to tag in case of Tag / Application Key Settings.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bOption | [In] Option to be used for information retrieval. One of the below values.
|
| [out] | ppResponse | [Out] Returns the key settings. |
| [out] | pRspLen | [Out] Length bytes available in ppKeySettings buffer. |
◆ phalNtagXDna_GetKeyVersion()
Reads out the current key version of any key stored on the tag.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bKeyNo | [In] Key number of the targeted key. |
| [out] | ppResponse | [Out] Key set versions of the selected application ordered by ascending key set number, i.e. starting with the AKS. |
| [out] | pRspLen | [Out] Length of bytes available in ppResponse buffer. |