Data Structures | |
| struct | phalVca_SamAV2_X_CardTableEntry_t |
| Data structure for Card table. More... | |
| struct | phalVca_SamAV2_X_IidTable_t |
| Structure for IID table IMPORTANT: Structure is reused to store RNDQ! More... | |
| struct | phalVca_SamAV2_X_KeysTable_t |
| Data structure for key entries. More... | |
| struct | phalVca_SamAV2_X_DataParams_t |
| Sw AL-VCA parameter structure. More... | |
| struct | phalVca_SamAV3_X_DataParams_t |
| SAMAV3 X AL-VCA parameter structure. More... | |
Macros | |
| #define | PHAL_VCA_SAMAV2_X_ID 0x02 |
| ID for SamAV2 Virtual Card Architecture layer. | |
| #define | PHAL_VCA_SAMAV3_X_ID 0x03 |
| ID for SamAV3 Virtual Card Architecture layer. | |
Functions | |
| phStatus_t | phalVca_SamAV2_X_Init (phalVca_SamAV2_X_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, phhalHw_SamAV2_DataParams_t *pSamHal, phpalMifare_SamAV2_X_DataParams_t *pPalMifareDataParams, phalVca_SamAV2_X_IidTable_t *pIidTable, phalVca_SamAV2_X_KeysTable_t *pKeysTable, uint16_t wNumIidKeysTableEntries, phalVca_SamAV2_X_CardTableEntry_t *pCardTableStorage, uint16_t wNumCardTableStorageEntries) |
| Initialization API for AL VCA / PC to communicate with SamAV2 in X Mode. More... | |
| phStatus_t | phalVca_SamAV3_X_Init (phalVca_SamAV3_X_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, phhalHw_SamAV3_DataParams_t *pSamHal, phpalMifare_SamAV3_X_DataParams_t *pPalMifareDataParams) |
| Initialization API for AL VCA / PC to communicate with SamAV3 in X Mode. More... | |
| phStatus_t phalVca_SamAV2_X_Init | ( | phalVca_SamAV2_X_DataParams_t * | pDataParams, |
| uint16_t | wSizeOfDataParams, | ||
| phhalHw_SamAV2_DataParams_t * | pSamHal, | ||
| phpalMifare_SamAV2_X_DataParams_t * | pPalMifareDataParams, | ||
| phalVca_SamAV2_X_IidTable_t * | pIidTable, | ||
| phalVca_SamAV2_X_KeysTable_t * | pKeysTable, | ||
| uint16_t | wNumIidKeysTableEntries, | ||
| phalVca_SamAV2_X_CardTableEntry_t * | pCardTableStorage, | ||
| uint16_t | wNumCardTableStorageEntries | ||
| ) |
Initialization API for AL VCA / PC to communicate with SamAV2 in X Mode.
| PH_ERR_SUCCESS | Operation successful. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | wSizeOfDataParams | [In] Specifies the size of the data parameter structure. |
| [in] | pSamHal | [In] Pointer to the parameter structure of the Sam HAL. |
| [in] | pPalMifareDataParams | [In] Pointer to the parameter structure of the palMifare layer. |
| [in] | pIidTable | [In] Pointer to the IidTable of the layer |
| [in] | pKeysTable | [In] Pointer to the KeysTable of the layer |
| [in] | wNumIidKeysTableEntries | [In] Indicates the size of the key/Iid table. |
| [in] | pCardTableStorage | [In] Pointer to the Card Table storage for the layer. |
| [in] | wNumCardTableStorageEntries | [In] Number of possible Card table entries in the storage. |
| phStatus_t phalVca_SamAV3_X_Init | ( | phalVca_SamAV3_X_DataParams_t * | pDataParams, |
| uint16_t | wSizeOfDataParams, | ||
| phhalHw_SamAV3_DataParams_t * | pSamHal, | ||
| phpalMifare_SamAV3_X_DataParams_t * | pPalMifareDataParams | ||
| ) |
Initialization API for AL VCA / PC to communicate with SamAV3 in X Mode.
| PH_ERR_SUCCESS | Operation successful. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | wSizeOfDataParams | [In] Specifies the size of the data parameter structure. |
| [in] | pSamHal | [In] Pointer to the parameter structure of the Sam HAL. |
| [in] | pPalMifareDataParams | [In] Pointer to the parameter structure of the palMifare layer. |