NXP Reader Library  v17.1.0.2535
Component : SAM

To communicate to SAM using Pegoda Reader or DUT readers. More...

Collaboration diagram for Component : SAM:

Modules

 Configuration
 

Data Structures

struct  phbalReg_Sam_DataParams_t
 Sam BAL parameter structure. More...
 

Macros

#define PHBAL_REG_SAM_ID   0x0AU
 ID for SAM component.
 

Functions

phStatus_t phbalReg_Sam_Init (phbalReg_Sam_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, void *pLowerBalDataParams, uint8_t *pAtrBuffer, uint16_t wAtrBufSize, uint8_t *pTxBuffer, uint16_t wTxBufSize, uint8_t *pRxBuffer, uint16_t wRxBufSize)
 Initialize the SAM BAL component. More...
 

Detailed Description

To communicate to SAM using Pegoda Reader or DUT readers.

Note
  • Implements SAM interface for Direct-Mode Communication.
    Needs to be linked between SAM HAL and the actual communication BAL that interfaces with the Pegoda or DUT readers.
  • By default TDA communication is configured. To enable I2C communication mode, use Set Config interface with Communication Type as configuration identifier and I2C as value.
  • Default 0x2B will be used as Slave Address and 200ms timeout for I2C Communication.

Function Documentation

◆ phbalReg_Sam_Init()

phStatus_t phbalReg_Sam_Init ( phbalReg_Sam_DataParams_t pDataParams,
uint16_t  wSizeOfDataParams,
void *  pLowerBalDataParams,
uint8_t pAtrBuffer,
uint16_t  wAtrBufSize,
uint8_t pTxBuffer,
uint16_t  wTxBufSize,
uint8_t pRxBuffer,
uint16_t  wRxBufSize 
)

Initialize the SAM BAL component.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
PH_ERR_INVALID_DATA_PARAMSParameter structure size is invalid.
PH_ERR_INVALID_PARAMETERwAtrBufSize, wTxBufSize or wRxBufSize is invalid.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]wSizeOfDataParams[In] Specifies the size of the data parameter structure.
[in]pLowerBalDataParams[In] Pointer to the BAL which actually connects to Pegoda or DUT reader in direct mode.
[in]pAtrBuffer[In] Pointer to buffer used for storing the ATR after card activation.
[in]wAtrBufSize[In] Size of the ATR buffer.
[in]pTxBuffer[In] Pointer to global transmit buffer used by the Exchange() function.
[in]wTxBufSize[In] Size of the global transmit buffer.
[in]pRxBuffer[In] Pointer to global receive buffer used by the Exchange() function.
[in]wRxBufSize[In] Size of the global receive buffer.