NXP Reader Library  v17.1.0.2535
Component : Stub

Component without functionality to ease implementation of additional busses. More...

Collaboration diagram for Component : Stub:

Data Structures

struct  phbalReg_Stub_DataParams_t
 BAL Stub parameter structure. More...
 

Macros

#define PHBAL_REG_STUB_ID   0x08U
 ID for Stub BAL component.
 

Functions

phStatus_t phbalReg_Stub_Init (phbalReg_Stub_DataParams_t *pDataParams, uint16_t wSizeOfDataParams)
 Initialise the BAL Stub layer. More...
 

Detailed Description

Component without functionality to ease implementation of additional busses.

Function Documentation

◆ phbalReg_Stub_Init()

phStatus_t phbalReg_Stub_Init ( phbalReg_Stub_DataParams_t pDataParams,
uint16_t  wSizeOfDataParams 
)

Initialise the BAL Stub layer.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
PH_ERR_INVALID_DATA_PARAMSParameter structure size is invalid.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]wSizeOfDataParams[In] Specifies the size of the data parameter structure.