Reader Initialization commands.
More...
|
| | Command_Codes |
| | Reader Initialization Command Codes of HAL DUT Command dispatcher frame.
|
| |
Reader Initialization commands.
◆ phhalHw_DUT_InitReader()
Performs the initialization of different Components.
To initialize the communication interface of the reader below information should be used for wCmd parameter.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | [IN] Pointer to this layer parameter structure. |
| [in] | wCmd | [IN] Command to initialize the Reader. Refer description for values and combination to use. |