Internal definitions. More...

Macros | |
| #define | PHHAL_HW_RC523_TIMER_FREQ 13.56f |
| RC internal timer frequency. | |
| #define | PHHAL_HW_RC523_TIMER_MAX_VALUE_US 39586813 |
| RC maximum timer value in microseconds. | |
| #define | PHHAL_HW_RC523_TIMER_SHIFT 4.8f |
| Shift of the internal RC timer in ETUs. | |
| #define | PHHAL_HW_RC523_ETU_106 9.44f |
| Duration of one ETU at 106 kBit/s in [us]. | |
| #define | PHHAL_HW_RC523_MFC_AUTHA_CMD 0x60U |
| MIFARE(R) Classic AUTHA command code. | |
| #define | PHHAL_HW_RC523_MFC_AUTHB_CMD 0x61U |
| MIFARE(R) Classic AUTHB command code. | |
Functions | |
| phStatus_t | phhalHw_Rc523_WriteFifo (phhalHw_Rc523_DataParams_t *pDataParams, uint8_t *pData, uint16_t wLength, uint16_t *pBytesWritten) |
| Write Data to Fifo buffer. More... | |
| phStatus_t | phhalHw_Rc523_ReadFifo (phhalHw_Rc523_DataParams_t *pDataParams, uint16_t wBufSize, uint8_t *pData, uint16_t *pLength) |
| Read Data from Fifo buffer. More... | |
| phStatus_t | phhalHw_Rc523_FlushFifo (phhalHw_Rc523_DataParams_t *pDataParams) |
| Clear Fifo buffer. More... | |
| phStatus_t | phhalHw_Rc523_WriteData (phhalHw_Rc523_DataParams_t *pDataParams, uint8_t bAddress, uint8_t *pData, uint16_t wLength) |
| Write multiple values to a single register address. More... | |
| phStatus_t | phhalHw_Rc523_ReadData (phhalHw_Rc523_DataParams_t *pDataParams, uint8_t bAddress, uint16_t wLength, uint8_t *pData) |
| Read multiple values from single register address. More... | |
| phStatus_t | phhalHw_Rc523_ExchangeTransmit (phhalHw_Rc523_DataParams_t *pDataParams, uint8_t bCmdCode, uint8_t *pTxBuffer, uint16_t wTxLength) |
| Transmit part of Exchange command. More... | |
| phStatus_t | phhalHw_Rc523_ExchangeReceive (phhalHw_Rc523_DataParams_t *pDataParams, uint8_t **ppRxBuffer, uint16_t *pRxLength) |
| Receive part of Exchange command. More... | |
| phStatus_t | phhalHw_Rc523_SetFdt (phhalHw_Rc523_DataParams_t *pDataParams, uint8_t bUnit, uint16_t wTimeout) |
| Sets the Frame Delay Time (Timeout). More... | |
| phStatus_t | phhalHw_Rc523_GetFdt (phhalHw_Rc523_DataParams_t *pDataParams, phStatus_t wExchangeStatus, uint32_t *pTime) |
| Retrieves the Frame Delay Time of the last command. More... | |
| phStatus_t | phhalHw_Rc523_GetTxBuffer (phhalHw_Rc523_DataParams_t *pDataParams, uint8_t bIsExchange, uint8_t **pTxBuffer, uint16_t *pTxBufferLen, uint16_t *pTxBufferSize) |
| Returns the TxBuffer pointer, length and size. More... | |
| phStatus_t | phhalHw_Rc523_GetRxBuffer (phhalHw_Rc523_DataParams_t *pDataParams, uint8_t bIsExchange, uint8_t **pRxBuffer, uint16_t *pRxBufferLen, uint16_t *pRxBufferSize) |
| Returns the RxBuffer pointer, length and size. More... | |
| phStatus_t | phhalHw_Rc523_WaitIrq (phhalHw_Rc523_DataParams_t *pDataParams, uint8_t bIrq0WaitFor, uint8_t bIrq1WaitFor, uint8_t *pIrq0Reg, uint8_t *pIrq1Reg) |
| Wait until one of the given interrupts occurs. More... | |
Timing related constants | |
| #define | PHHAL_HW_RC523_FELICA_ADD_DELAY_US 240U |
| Additional digital timeout delay for Felica. | |
RS232 speed settings | |
| #define | PHHAL_HW_RC523_SERIALSPEED_7200 0xFAU |
| 7.200 kBit/s. | |
| #define | PHHAL_HW_RC523_SERIALSPEED_9600 0xEBU |
| 9.600 kBit/s. | |
| #define | PHHAL_HW_RC523_SERIALSPEED_14400 0xDAU |
| 14.400 kBit/s. | |
| #define | PHHAL_HW_RC523_SERIALSPEED_19200 0xCBU |
| 19.200 kBit/s. | |
| #define | PHHAL_HW_RC523_SERIALSPEED_38400 0xABU |
| 38.400 kBit/s. | |
| #define | PHHAL_HW_RC523_SERIALSPEED_57600 0x9AU |
| 57.500 kBit/s. | |
| #define | PHHAL_HW_RC523_SERIALSPEED_115200 0x7AU |
| 115.200 kBit/s. | |
| #define | PHHAL_HW_RC523_SERIALSPEED_128000 0x74U |
| 128.000 kBit/s. | |
| #define | PHHAL_HW_RC523_SERIALSPEED_230400 0x5AU |
| 230.400 kBit/s. | |
| #define | PHHAL_HW_RC523_SERIALSPEED_460800 0x3AU |
| 460.800 kBit/s. | |
| #define | PHHAL_HW_RC523_SERIALSPEED_921600 0x1CU |
| 921.600 kBit/s. | |
| #define | PHHAL_HW_RC523_SERIALSPEED_1228800 0x15U |
| 1.228.800 kBit/s. | |
Internal definitions.
| phStatus_t phhalHw_Rc523_WriteFifo | ( | phhalHw_Rc523_DataParams_t * | pDataParams, |
| uint8_t * | pData, | ||
| uint16_t | wLength, | ||
| uint16_t * | pBytesWritten | ||
| ) |
Write Data to Fifo buffer.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | pData | [In] input data |
| [in] | wLength | [In] length of input data |
| [out] | pBytesWritten | [Out] Number of written bytes |
| phStatus_t phhalHw_Rc523_ReadFifo | ( | phhalHw_Rc523_DataParams_t * | pDataParams, |
| uint16_t | wBufSize, | ||
| uint8_t * | pData, | ||
| uint16_t * | pLength | ||
| ) |
Read Data from Fifo buffer.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | wBufSize | [In] size of output buffer |
| [out] | pData | [Out] output data |
| [out] | pLength | [Out] number of output data bytes |
| phStatus_t phhalHw_Rc523_FlushFifo | ( | phhalHw_Rc523_DataParams_t * | pDataParams | ) |
Clear Fifo buffer.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| phStatus_t phhalHw_Rc523_WriteData | ( | phhalHw_Rc523_DataParams_t * | pDataParams, |
| uint8_t | bAddress, | ||
| uint8_t * | pData, | ||
| uint16_t | wLength | ||
| ) |
Write multiple values to a single register address.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bAddress | [In] Start-Register Address |
| [in] | pData | [In] Register Values; uint8_t[wLength] |
| [in] | wLength | [In] Number of Values |
| phStatus_t phhalHw_Rc523_ReadData | ( | phhalHw_Rc523_DataParams_t * | pDataParams, |
| uint8_t | bAddress, | ||
| uint16_t | wLength, | ||
| uint8_t * | pData | ||
| ) |
Read multiple values from single register address.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bAddress | [In] Register Address |
| [in] | wLength | [In] Number of Values |
| [out] | pData | [Out] Register Values; uint8_t[wLength] |
| phStatus_t phhalHw_Rc523_ExchangeTransmit | ( | phhalHw_Rc523_DataParams_t * | pDataParams, |
| uint8_t | bCmdCode, | ||
| uint8_t * | pTxBuffer, | ||
| uint16_t | wTxLength | ||
| ) |
Transmit part of Exchange command.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bCmdCode | [In] Command-Code of command. |
| [in] | pTxBuffer | [In] Data to transmit. |
| [in] | wTxLength | [In] Length of data to transmit. |
| phStatus_t phhalHw_Rc523_ExchangeReceive | ( | phhalHw_Rc523_DataParams_t * | pDataParams, |
| uint8_t ** | ppRxBuffer, | ||
| uint16_t * | pRxLength | ||
| ) |
Receive part of Exchange command.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [out] | ppRxBuffer | [Out] Pointer to received data. |
| [out] | pRxLength | [Out] Number of received data bytes. |
| phStatus_t phhalHw_Rc523_SetFdt | ( | phhalHw_Rc523_DataParams_t * | pDataParams, |
| uint8_t | bUnit, | ||
| uint16_t | wTimeout | ||
| ) |
Sets the Frame Delay Time (Timeout).
Note: Frame Delay Time is defined between the last transmitted bit and the first received bit.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bUnit | [In] Unit of given timeout value (either PHHAL_HW_TIME_MICROSECONDS or PHHAL_HW_TIME_MILLISECONDS). |
| [in] | wTimeout | [In] Timeout value. |
| phStatus_t phhalHw_Rc523_GetFdt | ( | phhalHw_Rc523_DataParams_t * | pDataParams, |
| phStatus_t | wExchangeStatus, | ||
| uint32_t * | pTime | ||
| ) |
Retrieves the Frame Delay Time of the last command.
Note: Frame Delay Time is defined between the last transmitted bit and the first received bit.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | wExchangeStatus | [In] Status code returned by exchange function. |
| [out] | pTime | [Out] Calculated time in microseconds from timer contents. |
| phStatus_t phhalHw_Rc523_GetTxBuffer | ( | phhalHw_Rc523_DataParams_t * | pDataParams, |
| uint8_t | bIsExchange, | ||
| uint8_t ** | pTxBuffer, | ||
| uint16_t * | pTxBufferLen, | ||
| uint16_t * | pTxBufferSize | ||
| ) |
Returns the TxBuffer pointer, length and size.
| PH_ERR_SUCCESS | Operation successful. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bIsExchange | [In] Whether this is for Exchange (PH_ON) or not (PH_OFF). |
| [out] | pTxBuffer | [Out] Pointer to the TxBuffer. |
| [out] | pTxBufferLen | [Out] Number of bytes already in the TxBuffer. |
| [out] | pTxBufferSize | [Out] Size of the TxBuffer. |
| phStatus_t phhalHw_Rc523_GetRxBuffer | ( | phhalHw_Rc523_DataParams_t * | pDataParams, |
| uint8_t | bIsExchange, | ||
| uint8_t ** | pRxBuffer, | ||
| uint16_t * | pRxBufferLen, | ||
| uint16_t * | pRxBufferSize | ||
| ) |
Returns the RxBuffer pointer, length and size.
| PH_ERR_SUCCESS | Operation successful. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bIsExchange | [In] Whether this is for Exchange (PH_ON) or not (PH_OFF). |
| [out] | pRxBuffer | [Out] Pointer to the RxBuffer. |
| [out] | pRxBufferLen | [Out] Number of bytes already in the RxBuffer. |
| [out] | pRxBufferSize | [Out] Size of the RxBuffer. |
| phStatus_t phhalHw_Rc523_WaitIrq | ( | phhalHw_Rc523_DataParams_t * | pDataParams, |
| uint8_t | bIrq0WaitFor, | ||
| uint8_t | bIrq1WaitFor, | ||
| uint8_t * | pIrq0Reg, | ||
| uint8_t * | pIrq1Reg | ||
| ) |
Wait until one of the given interrupts occurs.
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bIrq0WaitFor | [In] Bitmask of interrupts in CommIrq register to wait for. |
| [in] | bIrq1WaitFor | [In] Bitmask of interrupts in DivIrq register to wait for. |
| [out] | pIrq0Reg | [Out] Contents of CommIrq register. |
| [out] | pIrq1Reg | [Out] Contents of DivIrq register. |