NXP Reader Library  v17.1.0.2535

RC632 Reader HAL. More...

Collaboration diagram for Component : Rc632:

Modules

 Commands
 Supported Reader commands.
 
 Internal
 Internal definitions.
 
 Register Definitions
 
 Configuration
 Custom Configuration of hardware related settings.
 

Data Structures

struct  phhalHw_Rc632_DataParams_t
 Rc632 HAL parameter structure. More...
 

Macros

#define PHHAL_HW_RC632_ID   0x09
 ID for Rc632 HAL component.
 
#define PHHAL_HW_RC632_SHADOW_COUNT   0x000DU
 Number of shadowed configurations.
 
#define PHHAL_HW_RC632_DEFAULT_TIMEOUT_MS   5U
 Default timeout in milliseconds.
 

Functions

phStatus_t phhalHw_Rc632_Init (phhalHw_Rc632_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, void *pBalDataParams, uint8_t *pTxBuffer, uint16_t wTxBufSize, uint8_t *pRxBuffer, uint16_t wRxBufSize)
 Initialise the HAL component. More...
 

Detailed Description

RC632 Reader HAL.

Function Documentation

◆ phhalHw_Rc632_Init()

phStatus_t phhalHw_Rc632_Init ( phhalHw_Rc632_DataParams_t pDataParams,
uint16_t  wSizeOfDataParams,
void *  pBalDataParams,
uint8_t pTxBuffer,
uint16_t  wTxBufSize,
uint8_t pRxBuffer,
uint16_t  wRxBufSize 
)

Initialise the HAL component.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlaying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]wSizeOfDataParams[In] Specifies the size of the data parameter structure.
[in]pBalDataParams[In] Pointer to the lower layers parameter structure.
[in]pTxBuffer[In] Pointer to global transmit buffer used by the Exchange() function.
[in]wTxBufSize[In] Size of the global transmit buffer.
[in]pRxBuffer[In] Pointer to global receive buffer used by the Exchange() function.
[in]wRxBufSize[In] Size of the global receive buffer. Specify the buffer +1 byte, because one byte is reserved for SPI communication.