NXP Reader Library  v17.1.0.2535

Provides a Secure Messaging interface for HostComm AV2. More...

Collaboration diagram for SamAV2:

Functions

phStatus_t phhalHw_SamAV2_Hc_AV2_AuthenticateHost (phhalHw_SamAV2_DataParams_t *pDataParams, uint8_t bAuthType, uint16_t wRdKeyRefNum, uint16_t wRdKeyRefVer, uint8_t bSamKeyRefNum, uint8_t bSamKeyRefVer)
 Perform Host Authentication Commands and responses using SamAV2 Host Protocol. More...
 
phStatus_t phhalHw_SamAV2_Hc_AV2_Int_Encrypt (phhalHw_SamAV2_DataParams_t *pDataParams, uint8_t *pBuffer, uint16_t wTxLength, uint16_t wBufferSize, uint16_t *pTxLength, uint8_t bFirst, uint8_t bLast)
 Perform Encryption using SamAV2 Host Protocol. More...
 
phStatus_t phhalHw_SamAV2_Hc_AV2_Int_Decrypt (phhalHw_SamAV2_DataParams_t *pDataParams, uint8_t *pBuffer, uint16_t wRxLength, uint16_t *pRxLength, uint8_t bFirst, uint8_t bLast)
 Perform Decryption using SamAV2 Host Protocol. More...
 
phStatus_t phhalHw_SamAV2_Hc_AV2_Int_AppendMac (phhalHw_SamAV2_DataParams_t *pDataParams, uint8_t *pBuffer, uint16_t wTxLength, uint16_t wBufferSize, uint16_t *pTxLength, uint8_t bFirst, uint8_t bLast)
 Append MAC to a data stream using SamAV2 Host Protocol. More...
 
phStatus_t phhalHw_SamAV2_Hc_AV2_Int_VerifyRemoveMac (phhalHw_SamAV2_DataParams_t *pDataParams, uint8_t *pBuffer, uint16_t wRxLength, uint16_t *pRxLength, uint8_t bFirst, uint8_t bLast)
 Remove Mac and verify it using SamAV2 Host Protocol. More...
 
phStatus_t phhalHw_SamAV2_Hc_AV2_Int_GetFirstLastCommand (phhalHw_SamAV2_DataParams_t *pDataParams, uint8_t bCmd, uint8_t bP1, uint8_t bP2, uint8_t *pFirstCmd, uint8_t *pLastCmd)
 
phStatus_t phhalHw_SamAV2_Hc_AV2_Int_GetFirstLastResponse (phhalHw_SamAV2_DataParams_t *pDataParams, uint8_t bSw1, uint8_t bSw2, uint8_t *pFirstResponse, uint8_t *pLastResponse)
 

Detailed Description

Provides a Secure Messaging interface for HostComm AV2.

Function Documentation

◆ phhalHw_SamAV2_Hc_AV2_AuthenticateHost()

phStatus_t phhalHw_SamAV2_Hc_AV2_AuthenticateHost ( phhalHw_SamAV2_DataParams_t pDataParams,
uint8_t  bAuthType,
uint16_t  wRdKeyRefNum,
uint16_t  wRdKeyRefVer,
uint8_t  bSamKeyRefNum,
uint8_t  bSamKeyRefVer 
)

Perform Host Authentication Commands and responses using SamAV2 Host Protocol.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlaying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]bAuthType[In] The type of Authentication to perform.
[in]wRdKeyRefNum[In] The key reference number for readerLib KeyStorage.
[in]wRdKeyRefVer[In] The key reference version for readerLib KeyStorage.
[in]bSamKeyRefNum[In] The key reference number for SAM KeyStorage.
[in]bSamKeyRefVer[In] The key reference version for SAM KeyStorage.

◆ phhalHw_SamAV2_Hc_AV2_Int_Encrypt()

phStatus_t phhalHw_SamAV2_Hc_AV2_Int_Encrypt ( phhalHw_SamAV2_DataParams_t pDataParams,
uint8_t pBuffer,
uint16_t  wTxLength,
uint16_t  wBufferSize,
uint16_t pTxLength,
uint8_t  bFirst,
uint8_t  bLast 
)

Perform Encryption using SamAV2 Host Protocol.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlaying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]pBuffer[In] Data to encrypt.
[in]wTxLength[In] Length of data to encrypt.
[in]wBufferSize[In] Size of the buffer.
[out]pTxLength[Out] Number of encrypted data bytes.
[in]bFirst[In] Whether this is the first block.
[in]bLast[In] Whether this is the last block.

◆ phhalHw_SamAV2_Hc_AV2_Int_Decrypt()

phStatus_t phhalHw_SamAV2_Hc_AV2_Int_Decrypt ( phhalHw_SamAV2_DataParams_t pDataParams,
uint8_t pBuffer,
uint16_t  wRxLength,
uint16_t pRxLength,
uint8_t  bFirst,
uint8_t  bLast 
)

Perform Decryption using SamAV2 Host Protocol.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlaying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]pBuffer[In] Data to decrypt.
[in]wRxLength[In] Length of data to decrypt.
[out]pRxLength[Out] Number of decrypted data bytes.
[in]bFirst[In] Whether this is the first block.
[in]bLast[In] Whether this is the last block.

◆ phhalHw_SamAV2_Hc_AV2_Int_AppendMac()

phStatus_t phhalHw_SamAV2_Hc_AV2_Int_AppendMac ( phhalHw_SamAV2_DataParams_t pDataParams,
uint8_t pBuffer,
uint16_t  wTxLength,
uint16_t  wBufferSize,
uint16_t pTxLength,
uint8_t  bFirst,
uint8_t  bLast 
)

Append MAC to a data stream using SamAV2 Host Protocol.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlaying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]pBuffer[In] Data to mac.
[in]wTxLength[In] Length of data to mac.
[in]wBufferSize[In] Size of the buffer.
[out]pTxLength[Out] Number of data bytes incl. MAC.
[in]bFirst[In] Whether this is the first block.
[in]bLast[In] Whether this is the last block.

◆ phhalHw_SamAV2_Hc_AV2_Int_VerifyRemoveMac()

phStatus_t phhalHw_SamAV2_Hc_AV2_Int_VerifyRemoveMac ( phhalHw_SamAV2_DataParams_t pDataParams,
uint8_t pBuffer,
uint16_t  wRxLength,
uint16_t pRxLength,
uint8_t  bFirst,
uint8_t  bLast 
)

Remove Mac and verify it using SamAV2 Host Protocol.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlaying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]pBuffer[In] data to unmac.
[in]wRxLength[In] length of data to unmac.
[out]pRxLength[Out] number of unmaced data bytes.
[in]bFirst[In] Whether this is the first block.
[in]bLast[In] Whether this is the last block.

◆ phhalHw_SamAV2_Hc_AV2_Int_GetFirstLastCommand()

phStatus_t phhalHw_SamAV2_Hc_AV2_Int_GetFirstLastCommand ( phhalHw_SamAV2_DataParams_t pDataParams,
uint8_t  bCmd,
uint8_t  bP1,
uint8_t  bP2,
uint8_t pFirstCmd,
uint8_t pLastCmd 
)
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]bCmd[In] Command code.
[in]bP1[In] P1 of command.
[in]bP2[In] P2 of command.
[out]pFirstCmd[Out] Whether this is the first block.
[out]pLastCmd[Out] Whether this is the last block.

◆ phhalHw_SamAV2_Hc_AV2_Int_GetFirstLastResponse()

phStatus_t phhalHw_SamAV2_Hc_AV2_Int_GetFirstLastResponse ( phhalHw_SamAV2_DataParams_t pDataParams,
uint8_t  bSw1,
uint8_t  bSw2,
uint8_t pFirstResponse,
uint8_t pLastResponse 
)
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]bSw1[In] SW1 of response.
[in]bSw2[In] SW2 of response.
[out]pFirstResponse[Out] Whether this is the first block.
[out]pLastResponse[Out] Whether this is the last block.