SAM commands used for ISO14443 layer 4 communication in X-Mode.
More...
|
| phStatus_t | phhalHw_SamAV2_Cmd_X_ISO14443_4_RATS_PPS (phhalHw_SamAV2_DataParams_t *pDataParams, uint8_t bCidIn, uint8_t bDsiIn, uint8_t bDriIn, uint8_t *pCidOut, uint8_t *pDsiOut, uint8_t *pDriOut, uint8_t *pAts) |
| | Perform a combined RATS and PPS to prepare a card for T=CL data exchange. More...
|
| |
| phStatus_t | phhalHw_SamAV2_Cmd_X_ISO14443_4_Init (phhalHw_SamAV2_DataParams_t *pDataParams, uint8_t bCid, uint8_t bDri, uint8_t bDsi, uint8_t bFwi, uint8_t bFsci) |
| | Perform a init of ISO-14443-4 layer (init T=CL protocol). More...
|
| |
| phStatus_t | phhalHw_SamAV2_Cmd_X_ISO14443_4_Exchange (phhalHw_SamAV2_DataParams_t *pDataParams, uint16_t wOption, uint8_t *pAppDataIn, uint8_t bLenAppData, uint8_t **ppAppDataOut, uint16_t *pAppDataOutLength) |
| | Perform an exchange bytes according ISO14443-4 T=CL protocol. More...
|
| |
| phStatus_t | phhalHw_SamAV2_Cmd_X_ISO14443_4_PresenceCheck (phhalHw_SamAV2_DataParams_t *pDataParams) |
| | Check if an activated card is still in the field. More...
|
| |
| phStatus_t | phhalHw_SamAV2_Cmd_X_ISO14443_4_Deselect (phhalHw_SamAV2_DataParams_t *pDataParams, uint8_t bFreeCid) |
| | Perform a Deselect command. More...
|
| |
| phStatus_t | phhalHw_SamAV2_Cmd_X_ISO14443_4_FreeCid (phhalHw_SamAV2_DataParams_t *pDataParams, uint8_t *pCid, uint8_t bCidLength) |
| | Free one or more currently assigned CIDs. More...
|
| |
SAM commands used for ISO14443 layer 4 communication in X-Mode.
◆ phhalHw_SamAV2_Cmd_X_ISO14443_4_RATS_PPS()
Perform a combined RATS and PPS to prepare a card for T=CL data exchange.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bCidIn | [In] CID to be sent. |
| [in] | bDsiIn | [In] DSI to be sent. |
| [in] | bDriIn | [In] DRI to be sent. |
| [out] | pCidOut | [Out] CID used (1 byte). |
| [out] | pDsiOut | [Out] DSI used (1 byte). |
| [out] | pDriOut | [Out] DRI used (1 byte). |
| [out] | pAts | [Out] Pointer to a buffer containing the received ATS. The length of the ATS can be found on the first position. |
◆ phhalHw_SamAV2_Cmd_X_ISO14443_4_Init()
Perform a init of ISO-14443-4 layer (init T=CL protocol).
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bCid | [In] CID to apply. |
| [in] | bDri | [In] Bit rate PCD -> PICC. |
| [in] | bDsi | [In] Bit rate PICC -> PCD |
| [in] | bFwi | [In] Frame waiting time indicator. |
| [in] | bFsci | [In] Frame size card indicator. |
◆ phhalHw_SamAV2_Cmd_X_ISO14443_4_Exchange()
Perform an exchange bytes according ISO14443-4 T=CL protocol.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | wOption | [In] Option parameter:
|
| [in] | pAppDataIn | [In] Buffer containing application data to sent. |
| [in] | bLenAppData | [In] Length of application data to sent. |
| [out] | ppAppDataOut | [Out] Pointer to buffer containing the data returned by the PICC. |
| [out] | pAppDataOutLength | [Out] Amount of valid bytes in ppAppDataOut. |
◆ phhalHw_SamAV2_Cmd_X_ISO14443_4_PresenceCheck()
Check if an activated card is still in the field.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
◆ phhalHw_SamAV2_Cmd_X_ISO14443_4_Deselect()
Perform a Deselect command.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bFreeCid | [In] Bitmask for deselect option.
|
◆ phhalHw_SamAV2_Cmd_X_ISO14443_4_FreeCid()
Free one or more currently assigned CIDs.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | pCid | [In] Buffer containing all CIDs to be freed. |
| [in] | bCidLength | [In] Length of the CID buffer (01h to 0Eh). |