NXP Reader Library  v17.1.0.2535
Component : SamAV3

SamAV3 Reader HAL. More...

Collaboration diagram for Component : SamAV3:

Modules

 Register Definitions for Rc523
 Register definitions for Rc663.
 
 Register Definitions for Rc663
 Register definitions for Rc663.
 
 Host Communication
 Host Communication.
 
 Command Interface
 Command Interface.
 

Data Structures

struct  phhalHw_SamAV3_DataParams_t
 SamAV3 HAL parameter structure. More...
 

Macros

#define PHHAL_HW_SAMAV3_ID   0x10
 ID for SamAV3 HAL component.
 
#define PHHAL_HW_SAMAV3_RESERVED_TX_BUFFER_LEN   6U
 Amount of needed and reserved memory for the protocol overhead.
 
#define PHHAL_HW_SAMAV3_RESERVED_RX_BUFFER_LEN   2U
 Amount of needed and reserved memory for the protocol overhead.
 

Functions

phStatus_t phhalHw_SamAV3_Init (phhalHw_SamAV3_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, void *pBalDataParams, void *pReaderHalDataParams, void *pKeyStoreDataParams, void *pCryptoENCDataParams, void *pCryptoMACDataParams, void *pCryptoRngDataParams, void *pPLUpload_CryptoENCDataParams, void *pPLUpload_CryptoMACDataParams, uint8_t bOpMode, uint8_t bLogicalChannel, uint8_t *pTxBuffer, uint16_t wTxBufSize, uint8_t *pRxBuffer, uint16_t wRxBufSize, uint8_t *pPLUploadBuf)
 Initialise the HAL component. More...
 
phStatus_t phhalHw_SamAV3_DetectMode (phhalHw_SamAV3_DataParams_t *pDataParams)
 Detect UID, AV2/AV3 mode and HostAuth settings. More...
 

Operation modes

#define PHHAL_HW_SAMAV3_OPMODE_NON_X   0x00
 Non-X operation mode.
 
#define PHHAL_HW_SAMAV3_OPMODE_X_RC523   0x01
 X-Mode operation (using Rc523).
 
#define PHHAL_HW_SAMAV3_OPMODE_X_RC663   0x02
 X-Mode operation (using Rc663).
 

Host-Communication modes

#define PHHAL_HW_SAMAV3_HC_AV2_MODE   0x02U
 Sam AV2 hardware is used.
 
#define PHHAL_HW_SAMAV3_HC_AV3_MODE   0x03U
 Sam AV3 hardware is used with sam in Un-Activated or Activated state.
 

Configs

#define PHHAL_HW_SAMAV3_CONFIG_HOSTMODE   (PH_CONFIG_CUSTOM_BEGIN + 0)
 Get / Set the Hostmode; (e.g. More...
 
#define PHHAL_HW_SAMAV3_CONFIG_DISABLE_NONX_CFG_MAPPING   (PH_CONFIG_CUSTOM_BEGIN + 1)
 Disables the mapping of standard-configs to the Reader HAL if set to PH_ON; Default is PH_OFF; Only applicable in NonX-Mode.
 

phhalHw_SamAV3 Custom Exchange Option Bits

#define PHHAL_HW_SAMAV3_EXCHANGE_NO_ENCIPHERING_BIT   0x0010U
 Suppress MIFARE Crypto enciphering of transmitted data.
 
#define PHHAL_HW_SAMAV3_EXCHANGE_NO_DECIPHERING_BIT   0x0020U
 Suppress deciphering of received MIFARE Crypto streams.
 

Detailed Description

SamAV3 Reader HAL.

Also supports AV2 backwards compatibility mode.

Macro Definition Documentation

◆ PHHAL_HW_SAMAV3_CONFIG_HOSTMODE

#define PHHAL_HW_SAMAV3_CONFIG_HOSTMODE   (PH_CONFIG_CUSTOM_BEGIN + 0)

Get / Set the Hostmode; (e.g.

PHHAL_HW_SAMAV3_HC_AV2_MODE).

Function Documentation

◆ phhalHw_SamAV3_Init()

phStatus_t phhalHw_SamAV3_Init ( phhalHw_SamAV3_DataParams_t pDataParams,
uint16_t  wSizeOfDataParams,
void *  pBalDataParams,
void *  pReaderHalDataParams,
void *  pKeyStoreDataParams,
void *  pCryptoENCDataParams,
void *  pCryptoMACDataParams,
void *  pCryptoRngDataParams,
void *  pPLUpload_CryptoENCDataParams,
void *  pPLUpload_CryptoMACDataParams,
uint8_t  bOpMode,
uint8_t  bLogicalChannel,
uint8_t pTxBuffer,
uint16_t  wTxBufSize,
uint8_t pRxBuffer,
uint16_t  wRxBufSize,
uint8_t pPLUploadBuf 
)

Initialise the HAL component.

The operation mode used is only dependend on the pReaderHalDataParams parameter.
If it's value is NULL X-Mode operation is performed, otherwise the HAL operates in Non-X Mode.
Non-X Mode Specific: It is not neccessary to do any (non-specific) calls to the linked Reader-HAL except an Init(),
the SamAV3 HAL will take over complete control of the linked Reader.
Specific initialisation like PHHAL_HW_CONFIG_BAL_CONNECTION or PHHAL_HW_CONFIG_SERIAL_BITRATE etc. though may be neccessary depending on the used HAL.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlaying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]wSizeOfDataParams[In] Specifies the size of the data parameter structure.
[in]pBalDataParams[In] Pointer to the lower layers parameter structure.
[in]pReaderHalDataParams[In] Pointer to a Reader-HAL in Non-X Mode. Can be NULL if X-Mode is intended.
[in]pKeyStoreDataParams[In] Pointer to the KeyStore used for Host Authentication.
[in]pCryptoENCDataParams[In] Pointer to the ENC crypto layers parameter structure.
[in]pCryptoMACDataParams[In] Pointer to the MAC crypto layers parameter structure.
[in]pCryptoRngDataParams[In] Pointer to the parameter structure of the CryptoRng layer.
pPLUpload_CryptoENCDataParamsPointer to the ENC crypto layers parameter structure. This will be used for ProgrammableLogic feature only.
pPLUpload_CryptoMACDataParamsPointer to the MAC crypto layers parameter structure. This will be used for ProgrammableLogic feature only.
[in]bOpMode[In] The desired operation mode
[in]bLogicalChannel[In] The desired logical channel for this HAL.
[in]pTxBuffer[In] Pointer to global transmit buffer.
[in]wTxBufSize[In] Size of the global transmit buffer.
[in]pRxBuffer[In] Pointer to global receive buffer.
[in]wRxBufSize[In] Size of the global receive buffer.
[in]pPLUploadBuf[In] Pointer to global PLUpload buffer.

◆ phhalHw_SamAV3_DetectMode()

phStatus_t phhalHw_SamAV3_DetectMode ( phhalHw_SamAV3_DataParams_t pDataParams)

Detect UID, AV2/AV3 mode and HostAuth settings.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.