Command Interface. More...

Modules | |
| SAM Status Codes | |
| Defines used accross the whole SAM implementation for the status codes returned by Sam hardware. | |
| SAM Custom Error Codes | |
| SamAV3 Custom Error Codes for the respective status codes returned by Sam hardwre. | |
| SAM Global values. | |
| SamAV3 Global macro values that are used for most of the commands. | |
| Security and Configuration | |
| SAM commands used for host communication and security related configuration. | |
| Key Management | |
| SAM commands used for key management related configuration. | |
| Data Processing | |
| SAM commands used for data processing. | |
| Public Key Infrastructure | |
| SAM commands used for asymmetric key management, signature handling and symmetric key updates based on PKI. | |
| Virtual Card | |
| end of defgroup phhalHw_SamAV3_Cmd_PKI | |
| MIFARE DESFire | |
| SAM commands used for MIFARE DESFire PICC communication in X and S Mode. | |
| MIFARE Plus | |
| SAM commands used for MIFARE Plus PICC communication in X and S Mode. | |
| MIFARE Classic | |
| SAM commands use for MIFARE Classic PICC communication in X and Non-X mode. | |
| MIFARE Ultralight | |
| SAM commands use for MIFARE Ultralight PICC communication in X and Non-X mode. | |
| Common | |
| SAM commands used for performing CommitReaderID in both X and S mode. | |
| ISO / IEC 29167-10 | |
| SAM commands used for ICODE DNA Authentication in Non-X-Mode. | |
| EMV Commands | |
| SAM command for EMV feature. | |
| Programmable Logic | |
| SAM commands used for Programmable Logic feature. | |
| Reader Chips | |
| SAM commands used for reader IC communication. | |
| ISO14443-3 | |
| SAM commands used for ISO14443 layer 3 communication in X-Mode. | |
| ISO14443-4 | |
| SAM commands used for ISO14443 layer 4 communication in X-Mode. | |
Command Interface.