SAM commands used for MIFARE DESFire PICC communication in X and S Mode. More...

Modules | |
| S Mode | |
| SAM commands used for MIFARE DESFire communication in S-Mode. | |
| X Mode | |
| SAM commands used for MIFARE DESFire communication in X-Mode. | |
Option macros for SAM AV3 Cmd.SAM_AuthenticatePICC, Cmd.SAM_IsoAuthenticatePICC, Cmd.DESFIRE_AuthenticatePICC command. | |
| #define | PHHAL_HW_CMD_SAMAV3_AUTH_MODE_D40_EV1 0x00 |
| Sam DESFire Authentication mode as D40 and EV1. | |
| #define | PHHAL_HW_CMD_SAMAV3_AUTH_MODE_EV2_FIRST_AUTH 0x80 |
| Sam DESFire Authentication mode as EV2 First. | |
| #define | PHHAL_HW_CMD_SAMAV3_AUTH_MODE_EV2_NON_FIRST_AUTH 0xC0 |
| Sam DESFire Authentication mode as EV2 Non First. | |
| #define | PHHAL_HW_CMD_SAMAV3_ALLOW_SECURE_MESSAGING 0x00 |
| Sam DESFire Allow Secure Messaging. | |
| #define | PHHAL_HW_CMD_SAMAV3_SUPPRESS_SECURE_MESSAGING 0x20 |
| Sam DESFire Supress Secure Messaging. More... | |
| #define | PHHAL_HW_CMD_SAMAV3_KDF_AV1 0x00 |
| Sam DESFire key derivation type as AV1. | |
| #define | PHHAL_HW_CMD_SAMAV3_KDF_AV1_DOUBLE_ENCRYPTION 0x00 |
| Sam DESFire key derivation type as AV1 double encryption round. | |
| #define | PHHAL_HW_CMD_SAMAV3_KDF_AV1_SINGLE_ENCRYPTION 0x08 |
| Sam DESFire key derivation type as AV1 single encryption round. | |
| #define | PHHAL_HW_CMD_SAMAV3_KDF_AV2 0x10 |
| Sam DESFire key derivation type as AV2. | |
| #define | PHHAL_HW_CMD_SAMAV3_KDF_RFU 0x18 |
| Sam DESFire key derivation type as RFU. | |
| #define | PHHAL_HW_CMD_SAMAV3_KEY_SELECTION_KEY_ENTRY_NUMBER 0x00 |
| Sam DESFire key selection by key entry number. | |
| #define | PHHAL_HW_CMD_SAMAV3_KEY_SELECTION_DESFIRE_KEY_NUMBER 0x02 |
| Sam DESFire key selection by DESFIRE key number. | |
| #define | PHHAL_HW_CMD_SAMAV3_KEY_DIVERSIFICATION_OFF 0x00 |
| Sam DESFire key derivation disabled. | |
| #define | PHHAL_HW_CMD_SAMAV3_KEY_DIVERSIFICATION_ON 0x01 |
| Sam DESFire key derivation enabled. | |
Option macros for Key to be used for when EV2 Authentication is selected. | |
| #define | PHHAL_HW_CMD_SAMAV3_AUTH_MODE_NONE 0x00 |
| Sam DESFire Auth mode as D40, EV1. | |
| #define | PHHAL_HW_CMD_SAMAV3_AUTH_MODE_EV2 0x00 |
| Sam DESFire Auth mode as EV2. | |
| #define | PHHAL_HW_CMD_SAMAV3_AUTH_MODE_LRP 0x01 |
| Sam DESFire Auth mode as LRP. | |
Option macros for ISO mode selection. | |
| #define | PHHAL_HW_CMD_SAMAV3_ISO_MODE_NATIVE 0x00 |
| Sam DESFire ISO mode selection for Native command set. | |
| #define | PHHAL_HW_CMD_SAMAV3_ISO_MODE_ISO7816 0x40 |
| Sam DESFire ISO mode selection for ISO 7816-4 command set. | |
| #define | PHHAL_HW_CMD_SAMAV3_ISO_MODE_ISO_AUTHENTICATION 0x80 |
| Sam DESFire ISO mode selection for Iso complaint Authentication. | |
| #define | PHHAL_HW_CMD_SAMAV3_TMRI_ISO_MODE_NATIVE 0x00 |
| Sam CommitReaderID ISO mode selection for Native command set. | |
| #define | PHHAL_HW_CMD_SAMAV3_TMRI_ISO_MODE_ISO7816 0x40 |
| Sam CommitReaderID ISO mode selection for ISO 7816-4 command set. | |
Option macros for SAM AV3 Cmd.SAM_ChangeKey command | |
| #define | PHHAL_HW_CMD_SAMAV3_DIV_METHOD_AV1 0x00 |
| Sam DESFire diversification method as AV1. | |
| #define | PHHAL_HW_CMD_SAMAV3_DIV_METHOD_AV2 0x20 |
| Sam DESFire diversification method as AV2. | |
| #define | PHHAL_HW_CMD_SAMAV3_KDF_SAMAV2_RFU 0x00 |
| Sam DESFire diversification method as RFU if its SAM AV2. | |
| #define | PHHAL_HW_CMD_SAMAV3_KDF_CURRENT_KEY_DOUBLE_ENCRYPTION 0x00 |
| Sam DESFire diversification method of current key for AV1 as double encryption. | |
| #define | PHHAL_HW_CMD_SAMAV3_KDF_CURRENT_KEY_SINGLE_ENCRYPTION 0x10 |
| Sam DESFire diversification method of current key for AV1 as single encryption. | |
| #define | PHHAL_HW_CMD_SAMAV3_KDF_NEW_KEY_DOUBLE_ENCRYPTION 0x00 |
| Sam DESFire diversification method of new key for AV1 as double encryption. | |
| #define | PHHAL_HW_CMD_SAMAV3_KDF_NEW_KEY_SINGLE_ENCRYPTION 0x08 |
| Sam DESFire diversification method of new key for AV1 as single encryption. | |
| #define | PHHAL_HW_CMD_SAMAV3_KDF_CURRENT_KEY_OFF 0x00 |
| Sam DESFire diversification usage for current key is disabled. | |
| #define | PHHAL_HW_CMD_SAMAV3_KDF_CURRENT_KEY_ON 0x04 |
| Sam DESFire diversification usage for current key is enabled. | |
| #define | PHHAL_HW_CMD_SAMAV3_KDF_NEW_KEY_OFF 0x00 |
| Sam DESFire diversification usage for new key is disabled. | |
| #define | PHHAL_HW_CMD_SAMAV3_KDF_NEW_KEY_ON 0x02 |
| Sam DESFire diversification usage for new key is enabled. | |
| #define | PHHAL_HW_CMD_SAMAV3_CRYPTO_MODE_DIFFERENT_KEY 0x00 |
| Sam DESFire crypto computation mode are different for target and auth keys. | |
| #define | PHHAL_HW_CMD_SAMAV3_CRYPTO_MODE_SAME_KEY 0x01 |
| Sam DESFire crypto computation mode are same for target and auth keys. | |
| #define | PHHAL_HW_CMD_SAMAV3_CMD_TYPE_CHANGE_KEY 0x00 |
| Sam DESFire Change Key command type as Change Key. | |
| #define | PHHAL_HW_CMD_SAMAV3_CMD_TYPE_CHANGE_KEY_EV2 0x20 |
| Sam DESFire Change Key command type as Change Key EV2. | |
| #define | PHHAL_HW_CMD_SAMAV3_MASTER_KEY_UPDATE_EXCLUDE_KEYTYPE 0x00 |
| Sam DESFire PICC Master key update to exclude key type in cryptogram. | |
| #define | PHHAL_HW_CMD_SAMAV3_MASTER_KEY_UPDATE_INCLUDE_KEYTYPE 0x10 |
| Sam DESFire PICC Master key update to include key type in cryptogram. More... | |
Option for Cmd.DESFire_CreateTMFilePICC command. | |
| #define | PHHAL_HW_CMD_SAMAV3_CREATE_TM_FILE_COMM_MODE_PLAIN 0x00 |
| Sam DESFire communication mode as Plain. | |
| #define | PHHAL_HW_CMD_SAMAV3_CREATE_TM_FILE_COMM_MODE_MAC 0x01 |
| Sam DESFire communication mode as MAC. | |
| #define | PHHAL_HW_CMD_SAMAV3_CREATE_TM_FILE_COMM_MODE_FULL 0x03 |
| Sam DESFire communication mode as Full. | |
| #define | PHHAL_HW_CMD_SAMAV3_CREATE_TM_FILE_AES_KEY 0x02 |
| Sam DESFire TMKeyOption as AES. | |
SAM commands used for MIFARE DESFire PICC communication in X and S Mode.
| #define PHHAL_HW_CMD_SAMAV3_SUPPRESS_SECURE_MESSAGING 0x20 |
Sam DESFire Supress Secure Messaging.
To be used if originality keys are used.
| #define PHHAL_HW_CMD_SAMAV3_MASTER_KEY_UPDATE_INCLUDE_KEYTYPE 0x10 |
Sam DESFire PICC Master key update to include key type in cryptogram.
This byte will be right shifted 2 time to update the bit 4.