Data Structures | |
| struct | phpalI14443p4a_Pcsc_DataParams_t |
| PCSC ISO14443-4A parameter structure. More... | |
Macros | |
| #define | PHPAL_I14443P4A_PCSC_ID 0x05 |
| ID for PCSC ISO14443-4A layer | |
Functions | |
| phStatus_t | phpalI14443p4a_Pcsc_Init (phpalI14443p4a_Pcsc_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, void *pHalDataParams) |
| Initialise PCSC ISO14443-4A layer. More... | |
| phStatus_t phpalI14443p4a_Pcsc_Init | ( | phpalI14443p4a_Pcsc_DataParams_t * | pDataParams, |
| uint16_t | wSizeOfDataParams, | ||
| void * | pHalDataParams | ||
| ) |
Initialise PCSC ISO14443-4A layer.
| PH_ERR_SUCCESS | Operation successful. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | wSizeOfDataParams | [In] Specifies the size of the data parameter structure. |
| [in] | pHalDataParams | [In] Pointer to the parameter structure of HAL layer. |