NXP Reader Library  v17.1.0.2535

Component without functionality to ease implementation of additional busses. More...

Collaboration diagram for Component : Stub:

Data Structures

struct  phpalMifare_Stub_DataParams_t
 Stub PAL-MIFARE parameter structure. More...
 

Macros

#define PHPAL_MIFARE_STUB_ID   0x01
 ID for Stub MIFARE layer.
 

Functions

phStatus_t phpalMifare_Stub_Init (phpalMifare_Stub_DataParams_t *pDataParams, uint16_t wSizeOfDataParams)
 Initialise this layer. More...
 

Detailed Description

Component without functionality to ease implementation of additional busses.

Function Documentation

◆ phpalMifare_Stub_Init()

phStatus_t phpalMifare_Stub_Init ( phpalMifare_Stub_DataParams_t pDataParams,
uint16_t  wSizeOfDataParams 
)

Initialise this layer.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]wSizeOfDataParams[In] Specifies the size of the data parameter structure.