NXP Reader Library  v17.1.0.2535

Common commands that performs Activation of the VICC, Exchange to VICC, etc... More...

Collaboration diagram for Commands_Commmon:

Functions

phStatus_t phpalSli15693_ActivateCard (void *pDataParams, uint8_t bOption, uint8_t bFlags, uint8_t bAfi, uint8_t *pMask, uint8_t bMaskBitLen, uint8_t *pDsfid, uint8_t *pUid, uint8_t *pMoreCardsAvailable)
 Perform ISO15693 ActivateCard command. More...
 
phStatus_t phpalSli15693_SendEof (void *pDataParams, uint8_t bOption, uint8_t *pDsfid, uint8_t *pUid, uint8_t *pUidLen, uint8_t *pData, uint16_t *pDataLen)
 Send a ISO15693 EOF (End of Frame). More...
 
phStatus_t phpalSli15693_Exchange (void *pDataParams, uint16_t wOption, uint8_t *pTxBuffer, uint16_t wTxBuffLen, uint8_t **ppRxBuffer, uint16_t *pRxBuffLen)
 Perform ISO15693 Data Exchange with VICC. More...
 

Detailed Description

Common commands that performs Activation of the VICC, Exchange to VICC, etc...

Function Documentation

◆ phpalSli15693_ActivateCard()

phStatus_t phpalSli15693_ActivateCard ( void *  pDataParams,
uint8_t  bOption,
uint8_t  bFlags,
uint8_t  bAfi,
uint8_t pMask,
uint8_t  bMaskBitLen,
uint8_t pDsfid,
uint8_t pUid,
uint8_t pMoreCardsAvailable 
)

Perform ISO15693 ActivateCard command.

  • This function activates the first VICC detected during the collision resolution and optionally move it to selected state based on the wOption specified.
  • bOption can be one of:
Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
PH_ERR_INVALID_DATA_PARAMSIf DataParams is null.
PH_ERR_INVALID_PARAMETERIf the buffers are null.
PH_ERR_PROTOCOL_ERRORInvalid response received.
XXXX
  • Depending on status codes return by PICC.
  • Other Depending on implementation and underlying component.
Parameters
[in]pDataParams[In] Pointer to this layers parameter structure.
[in]bOption[In] Selected or addressed. Refer description for supported options.
[in]bFlags[In] Request flags byte. Refer below set of flags
[in]bAfi[In] Application Family Identifier.
[in]pMask[In] UID mask, holding known UID bits.
[in]bMaskBitLen[In] Number of UID bits within pMask.
[out]pDsfid[Out] Data Storage Format Identifier.
[out]pUid[Out] Received UID of first found card
[out]pMoreCardsAvailable[Out] If there are more cards available this value is different from zero.

◆ phpalSli15693_SendEof()

phStatus_t phpalSli15693_SendEof ( void *  pDataParams,
uint8_t  bOption,
uint8_t pDsfid,
uint8_t pUid,
uint8_t pUidLen,
uint8_t pData,
uint16_t pDataLen 
)

Send a ISO15693 EOF (End of Frame).

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
PH_ERR_INVALID_DATA_PARAMSIf DataParams is null.
PH_ERR_INVALID_PARAMETERIf the buffers are null.
PH_ERR_PROTOCOL_ERRORInvalid response received.
XXXX
  • Depending on status codes return by PICC.
  • Other Depending on implementation and underlying component.
Parameters
[in]pDataParams[In] Pointer to this layers parameter structure.
[in]bOption[In] Option parameter. Refer description for supported options.
[out]pDsfid[Out] Data Storage Format Identifier.
[out]pUid[Out] Received UID
[out]pUidLen[Out] Length of bytes available in pUid buffer.
[out]pData[Out] Received data.
[out]pDataLen[Out] Length of bytes available in pData buffer.

◆ phpalSli15693_Exchange()

phStatus_t phpalSli15693_Exchange ( void *  pDataParams,
uint16_t  wOption,
uint8_t pTxBuffer,
uint16_t  wTxBuffLen,
uint8_t **  ppRxBuffer,
uint16_t pRxBuffLen 
)

Perform ISO15693 Data Exchange with VICC.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
PH_ERR_INVALID_DATA_PARAMSIf DataParams is null.
PH_ERR_INVALID_PARAMETERIf the buffers are null.
PH_ERR_PROTOCOL_ERRORInvalid response received.
XXXX
  • Depending on status codes return by PICC.
  • Other Depending on implementation and underlying component.
Parameters
[in]pDataParams[In] Pointer to this layers parameter structure.
[in]wOption[In] Buffering options. Refer description for supported options.
[in]pTxBuffer[In] Data to be transmitted to VICC.
Note
: Flags, IC MFC code and UID will be added automatically by the library internally.
Parameters
[in]wTxBuffLen[In] Length of bytes available in pTxBuffer buffer.
[out]ppRxBuffer[Out] Received information from VICC.
[out]pRxBuffLen[Out] Length of bytes available in ppRxBuffer buffer.