NXP Reader Library  v17.1.0.2535

Description of options to be used for Custom command sets. More...

Collaboration diagram for Defines:

Modules

 ExtendedInventoryFlags
 Description of extended flags. These flags should be used for the below mentioned commands.
 

Detailed Description

Description of options to be used for Custom command sets.