NXP Reader Library  v17.1.0.2535

Configuration and Option definitions. These options shall be used along with SetConfig and GetConfig to configure PAL Sli15693 layer. More...

Collaboration diagram for Defines:

Macros

#define PHPAL_SLI15693_CONFIG_FLAGS   0x0000U
 Set or get the flags byte. More...
 
#define PHPAL_SLI15693_CONFIG_ADD_INFO   0x0001U
 Get the additional info word. More...
 
#define PHPAL_SLI15693_CONFIG_TIMEOUT_US   0x0002U
 Set or get the current timeout in microseconds.
 
#define PHPAL_SLI15693_CONFIG_TIMEOUT_MS   0x0003U
 Set or get the current timeout in milliseconds.
 
#define PHPAL_SLI15693_CONFIG_TXDATARATE   0x0004U
 Set or get the current TX Data rate.
 
#define PHPAL_SLI15693_CONFIG_RXDATARATE   0x0005U
 Set or get the current RX Data rate.
 
#define PHPAL_SLI15693_CONFIG_T1_PARAMETER   0x0006U
 Set or get the current T1 timeout after Parameter Select.
 
#define PHPAL_SLI15693_CONFIG_ENABLE_BUFFERING   0x0007U
 Option to Get / Set the buffering of response data to be enabled or disabled. More...
 
#define PHPAL_SLI15693_CONFIG_MAXRETRYCOUNT   0x0008U
 Set / Get Maximum Retry Count.
 
#define PHPAL_SLI15693_CONFIG_ICMFGCODE   0x0009U
 Set / Get IC Manufacturer Code.
 
#define PHPAL_SLI15693_CONFIG_TRANSPARENT   0x0010U
 Set or get the Transparent mode.
 

Detailed Description

Configuration and Option definitions. These options shall be used along with SetConfig and GetConfig to configure PAL Sli15693 layer.

Macro Definition Documentation

◆ PHPAL_SLI15693_CONFIG_FLAGS

#define PHPAL_SLI15693_CONFIG_FLAGS   0x0000U

Set or get the flags byte.

This shall be used to set or get the value of Request Flag field used in the commands sent by the library.

◆ PHPAL_SLI15693_CONFIG_ADD_INFO

#define PHPAL_SLI15693_CONFIG_ADD_INFO   0x0001U

Get the additional info word.

This shall be used to set or get the value of Response Flag for authentication commands or the error code field used in the response received by the library.

◆ PHPAL_SLI15693_CONFIG_ENABLE_BUFFERING

#define PHPAL_SLI15693_CONFIG_ENABLE_BUFFERING   0x0007U

Option to Get / Set the buffering of response data to be enabled or disabled.

By default this flag will be disabled.