NXP Reader Library  v17.1.0.2535
phCidManager_Rd710_DataParams_t Struct Reference

Cid Manager parameter structure. More...

Data Fields

uint16_t wId
 Layer ID for this component, NEVER MODIFY!
 
phhalHw_Rd710_DataParams_tpHalDataParams
 [In] Pointer to the parameter structure of the underlying layer.
 

Detailed Description

Cid Manager parameter structure.


The documentation for this struct was generated from the following file: