NXP Reader Library  v17.1.0.2535
phCidManager_Sw_DataParams_t Struct Reference

Cid Manager parameter structure. More...

Data Fields

uint16_t wId
 Layer ID for this component, NEVER MODIFY!
 
uint8_t bCidList [PH_CIDMANAGER_LAST_CID]
 Contains a list of Cids, where a value of /c 0 means free and a value of /c 1 means occupied.
 

Detailed Description

Cid Manager parameter structure.


The documentation for this struct was generated from the following file: